Read announcements related to Remote Operations (formerly SCADA & Telemetry). New products, new versions, case studies, videos and other relevant news will be posted in this blog. Keep up-to-date with the challenges that remote sites present and how to ensure reliable communications, monitoring & management to enhance productivity and profitability.
Search in
Link copied. Please paste this link to share this article on your social media post.
Originally published on Remote Operations Blog by Joel_Weder | August 10, 2023 09:39 PM
Hello Remote Operations community,
Building on the RemoteConnect Ease-of-Use video playlist, this new video demonstrates the many diagnostic features available in RemoteConnect for the SCADAPack x70 model RTU's. RemoteConnect allows you to view system information and status objects from the online Diagnostics user interface, through object browsers within the software, and to make use of diagnostic parameters in the Logic Editor. Also, diagnostics may be viewed using the command line interface, which can be accessed via Telnet or serially, if enabled.
The SCADAPack 47xi Remote Smart RTU and Controller with Integrated Edge Platform is the latest model in the SCADAPack x70 series, combining wide-ranging RTU capabilities with the flexibility of Linux.
Video link: RemoteConnect Ease-of-Use - Online Diagnostics
RemoteConnect Ease-of-Use YouTube playlist link
Link copied. Please paste this link to share this article on your social media post.
All registered members have full access to the Community and can post comments and start topics.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.