New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Read announcements related to Remote Operations (formerly SCADA & Telemetry). New products, new versions, case studies, videos and other relevant news will be posted in this blog. Keep up-to-date with the challenges that remote sites present and how to ensure reliable communications, monitoring & management to enhance productivity and profitability.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Originally published on Remote Operations Blog by wmoulton | February 25, 2020 06:12 PM
“Ours is too small” you say. Is it?
For a second, let’s consider what these cybercriminals stand to gain from you: financial, data (operational, client, etc.), bandwidth, processing, and power. You likely thought of the first few – but have you considered how much processing power you could also be offering?
Why would processing, power and bandwidth be of interest? Cryptocurrency mining. It’s a constant game of measuring energy input (processing power) versus output of mined currency value. You also must consider the hardware costs involved with having specialized equipment to carry out the mining tasks.
Hackers are targeting corporations, utilities, and municipalities that have extensive processing abilities in place to run their business or service. With access to these power, processing and bandwidth resources, hackers can remove the expense side of their profit calculations, where regardless of the cost of energy to mine, when it’s free, it will always be worth it.
Water & Wasterwater utilities are at a particular disadvantage because there are always so many distributed assets that need to be monitored and controlled. With the ever-increasing downward pressure on expenditures, utilities must rely on remote monitoring in order to make the most effective use of their resources. These distributed assets, will typically have some kind of edge node(s) and communication path back to the Supervisory Control and Data Acquisition (SCADA) system.
Because these systems sit on the edge of the network, that opens them to the most risk for intrusion. Should we shut it all down, go off-grid, and revert to paper records? No. There are awesome advantages to having smart connected infrastructure, and they can empower your utility to realize true gains. With that to gain, special consideration needs to be given to the edge nodes and network that is going to be deployed at the edge.
So, what steps should you take to protect your Water & Wastewater network? Get to know the manufacturer of the hardware and software you choose. Using a defense-in-depth approach to all layers of your edge network starting from your connected products, your edge control, and the smart software that gives you your operational advantages can also offer you confidence that your system is secure. The cybersecurity story is not a destination, it is a journey that needs constant attention and will continue to evolve.
We are living in a time where automation hardware obsolescence speed is increasing – not because the hardware or software is failing – but because of the system’s ability to cope with next generation cybersecurity features, communication standards, and its ability to be compatible with security patches.
There are many reasons that a hacker would target a Water and Wastewater utility, with one of them being a cheap way to generate cryptocurrency. You can operate in a cybersecure way without completely disconnecting from the world – observe a defense-in-depth approach and a manufacturer that understands cybersecurity and its application in #SCADA & Telemetry networks.
We have a dedicated Cybersecurity services team, and SCADA & Telemetry expertise to help you on your journey of operating a robust and secure Water & Wastewater Network. Our experts are ready to answer your questions and technical issue on Geo SCADA Expert forum and SCADA and Telemetry Devices forum and if you want to discuss this topic further, feel free to leave me a comment below.
Never miss any update by subscribing to our SCADA and Telemetry Blog
Originally posted on SE Blog
Link copied. Please paste this link to share this article on your social media post.
All registered members have full access to the Community and can post comments and start topics.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.