Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PowerLogic T300 - Retrofit Underground FCI in Padmount Switchgear (US)

Protection & Control

Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
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
  • EcoStruxure Power & Grid
  • Protection & Control
  • PowerLogic T300 - Retrofit Underground FCI in Padmount Switchgear (US)
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Araceli_Monje
Araceli_Monje Mentor
60
Arun-kumar_PS
Arun-kumar_PS Mentor
26
JuanRayo
JuanRayo Mentor
24
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Related Products
product field
Schneider Electric
PowerLogic T300

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Protection & Control
Start a Topic
Solved
Chris_Kerr
Chris_Kerr Explorer
Explorer

Posted: ‎2021-04-08 04:24 PM . Last Modified: ‎2025-05-26 12:55 AM

1 Like
1
1356
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
‎2021-04-08 04:24 PM

PowerLogic T300 - Retrofit Underground FCI in Padmount Switchgear (US)

First time enlisting help from Exchange. 

 

We have a customer we are working with to try to develop a solution to use the T300 as an advanced underground FCI. 

 

Is it even feasible to use the T300 in a retrofit application where no sensors (CT's, PT's, or power to power a PS50 or DC power) is available? 

 

I'm curious what people's thoughts on the best way to integrate with for example S&C PME / PMH switchgear or some other manually operated gear if we want to get fault detection and communicate in real time (and the other benefits of the T300)?

 

 

  • Thumbnail of PowerLogic T300
    Schneider Electric
    PowerLogic T300
View products (1)
Labels
  • Labels:
  • PowerLogic T300
Tags (2)
  • Tags:
  • english
  • PowerLogic T300
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
JYPOC
JYPOC Mentor
Mentor

Posted: ‎2021-04-27 04:53 AM . Last Modified: ‎2021-04-27 04:55 AM

0
1346
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
‎2021-04-27 04:53 AM

Hi Chris,

 

First, it is important to remember that the SC150 module performs a 3-phase MV fault detection (ANSI 50/51/67 and 50N/51N/ 67N) and not a single-phase one.

 

Then to answer your questions:

 

1. To detect MV fault currents on solidly grounded MV network (typical US case) or resistor-earthed, you only need to add 3 phase measurement CTs (ranging from 50 to 1250 A on the primary side, and 1 or 5A on the secondary side). In addition, if you want to detect SEF down to 0.5 A, you will also need a 4th CT (core balanced CT, preferably 50/1 or so). Outside NA, we can offer 500/1 Class 1 or 3 CTs as they are fitted for the MV switchgear used: they have never been tested in the US (tbc) so I don't believe we can propose them. So you'll have to purchase these CTs from local US suppliers.

 

2. To detect directional earth faults and/or perform PM/PQ measurement, it is required to have 3 single-phase voltage measurements.

Outside North America, the MV switchgear is always fitted with a capacitive divider connected to the 3 MV capacitors of the MV switchgear. SE provides something called VPIS-VO V3 (voltage presence indicator system with voltage output) while German-influenced competitors utilize VDS (voltage detection system) but they can both be connected to the SC150-LPVT to perform directional fault detection, PM/PQ measurements, ANSI 29/59, ANSI 47BC and ANSI 32P (active overpower direction detection, very useful when many DER are deployed).

For retrofit in the US, I see two options: install either 3 LPVTs (1 per phase) or one 3-phase VT to the MV functions on which it is required to perform the above-mentionned features.

 

Regards,

BR - Jean-Yves

See Answer In Context

  • Thumbnail of PowerLogic T300
    Schneider Electric
    PowerLogic T300
View products (1)
Tags (4)
  • Tags:
  • enhanced FCI
  • SC150-LPVT
  • t300
  • US distribution automation
Reply
Reply 1
JYPOC
JYPOC Mentor
Mentor

Posted: ‎2021-04-27 04:53 AM . Last Modified: ‎2021-04-27 04:55 AM

0
1347
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
‎2021-04-27 04:53 AM

Hi Chris,

 

First, it is important to remember that the SC150 module performs a 3-phase MV fault detection (ANSI 50/51/67 and 50N/51N/ 67N) and not a single-phase one.

 

Then to answer your questions:

 

1. To detect MV fault currents on solidly grounded MV network (typical US case) or resistor-earthed, you only need to add 3 phase measurement CTs (ranging from 50 to 1250 A on the primary side, and 1 or 5A on the secondary side). In addition, if you want to detect SEF down to 0.5 A, you will also need a 4th CT (core balanced CT, preferably 50/1 or so). Outside NA, we can offer 500/1 Class 1 or 3 CTs as they are fitted for the MV switchgear used: they have never been tested in the US (tbc) so I don't believe we can propose them. So you'll have to purchase these CTs from local US suppliers.

 

2. To detect directional earth faults and/or perform PM/PQ measurement, it is required to have 3 single-phase voltage measurements.

Outside North America, the MV switchgear is always fitted with a capacitive divider connected to the 3 MV capacitors of the MV switchgear. SE provides something called VPIS-VO V3 (voltage presence indicator system with voltage output) while German-influenced competitors utilize VDS (voltage detection system) but they can both be connected to the SC150-LPVT to perform directional fault detection, PM/PQ measurements, ANSI 29/59, ANSI 47BC and ANSI 32P (active overpower direction detection, very useful when many DER are deployed).

For retrofit in the US, I see two options: install either 3 LPVTs (1 per phase) or one 3-phase VT to the MV functions on which it is required to perform the above-mentionned features.

 

Regards,

BR - Jean-Yves
  • Thumbnail of PowerLogic T300
    Schneider Electric
    PowerLogic T300
View products (1)
Tags (4)
  • Tags:
  • enhanced FCI
  • SC150-LPVT
  • t300
  • US distribution automation
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.