Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

P3 binary input threshold

Protection & Control

Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
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
  • EcoStruxure Power & Grid
  • Protection & Control
  • P3 binary input threshold
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Araceli_Monje
Commander Araceli_Monje Commander
43
Arun-kumar_PS
Commander Arun-kumar_PS Commander
21
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Related Products
product field
PowerLogic
PowerLogic P2

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Protection & Control
Start a Topic
Solved
palak
Lt. Commander palak Lt. Commander
Lt. Commander

Posted: ‎2021-04-13 08:41 PM . Last Modified: ‎2023-05-30 10:01 PM

0 Likes
1
1845
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
‎2021-04-13 08:41 PM

P3 binary input threshold

Easergy P3 relays binary inputs are rated form 24 to 255 VAC/DC with binary threshold link to order code as 24 VDC/110 VDC/220 VDC. question is even if we select 24 VDC in order code for all application then whatever the control voltage DI will activate so what is the reason or application when we select different threshold voltage.  for 110 VDC system would it be ok to select threshold as 24 VDC or it should be 110 VDC? 

 

  • Thumbnail of PowerLogic P2
    PowerLogic
    PowerLogic P2
View products (1)
Labels
  • Labels:
  • PowerLogic P3
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Rudolf_Simon
Commander Rudolf_Simon Commander
Commander

Posted: ‎2021-04-13 11:57 PM

0 Likes
0
1840
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
‎2021-04-13 11:57 PM

The need of higher binary input switching thresholds (> 50 % Vaux.nom) is independent from the relay platform.

The technical problem is illustrated in the figure below.  It is of relevance if the station supply battery is either set up with 2 segments and the neutral is grounded via a high resistance, or the DC circuit is equipped with an earth-fault monitoring device.  Then under certain earth-fault conditions (fault location as shown in the figure in the attached pdf) a voltage is present across the binary input of about half nominal battery voltage and a small current flows (practically determined by the resistances of the monitoring circuit and the opto-coupler input).  Under this condition, a wide-range opto-coupler input would pick up. 

 
 

One solution to prevent the false operation of the input under this condition is to have an operating threshold above half nominal battery voltage.

Another (‘classical’) solution is to use 2-pole switching on the few critical inputs (like intertripping inputs) – per 2nd sketch in the pdf.

 

In any case immediate action is recommended in case of bad isolation state of the battery supply system.

 

 

 

See Answer In Context

Attachments
Tags (1)
  • Tags:
  • english
Reply
Reply 1
Rudolf_Simon
Commander Rudolf_Simon Commander
Commander

Posted: ‎2021-04-13 11:57 PM

0 Likes
0
1841
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
‎2021-04-13 11:57 PM

The need of higher binary input switching thresholds (> 50 % Vaux.nom) is independent from the relay platform.

The technical problem is illustrated in the figure below.  It is of relevance if the station supply battery is either set up with 2 segments and the neutral is grounded via a high resistance, or the DC circuit is equipped with an earth-fault monitoring device.  Then under certain earth-fault conditions (fault location as shown in the figure in the attached pdf) a voltage is present across the binary input of about half nominal battery voltage and a small current flows (practically determined by the resistances of the monitoring circuit and the opto-coupler input).  Under this condition, a wide-range opto-coupler input would pick up. 

 
 

One solution to prevent the false operation of the input under this condition is to have an operating threshold above half nominal battery voltage.

Another (‘classical’) solution is to use 2-pole switching on the few critical inputs (like intertripping inputs) – per 2nd sketch in the pdf.

 

In any case immediate action is recommended in case of bad isolation state of the battery supply system.

 

 

 

Attachments
Tags (1)
  • Tags:
  • english
Reply
Preview Exit Preview

never-displayed

You must be signed in to add attachments

never-displayed
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.