PowerLogic T300 - IEC 104 protocol: how to achieve MSP-to-MDP conversion?

Protection & Control

Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
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
  • EcoStruxure Power & Grid
  • Protection & Control
  • PowerLogic T300 - IEC 104 protocol: how to achieve MSP-to-MDP conversion?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Araceli_Monje
Commander Araceli_Monje Commander
43
Arun-kumar_PS
Commander Arun-kumar_PS Commander
21
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Related Products
product field
Schneider Electric
PowerLogic T300

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Protection & Control
Start a Topic
John_Archer1
Ensign John_Archer1
Ensign

Posted: ‎2024-07-03 01:22 AM . Last Modified: ‎2024-07-09 04:12 AM

0 Likes
5
1623
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
‎2024-07-03 01:22 AM

PowerLogic T300 - IEC 104 protocol: how to achieve MSP-to-MDP conversion?

Hello guys, good day. I read the 104 protocol on the t300 rtu as single point and converted it to double point ABB rtu. It says it's being converted, but the wrong value is being sent

  • Thumbnail of PowerLogic T300
    Schneider Electric
    PowerLogic T300
View products (1)
Attachments
Labels
  • Labels:
  • PowerLogic T300
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 5
TomBerry
Lieutenant JG TomBerry Lieutenant JG
Lieutenant JG

Posted: ‎2024-07-04 01:29 AM

1 Like
0
1601
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
‎2024-07-04 01:29 AM

I see from the screen shot that the source coordinate is of type MSP and the destination coordinate has type MDP.  These coordinates tell the software what format to use in the protocol messages, but they don't translate the values.
MSP has values 0,1 = open/close MDP uses values 0,1,2,3 = intermediate/open/close/bad

What is needed is an intermediate variable with a formula.
There are built-in formulas to convert the value from SPS to DPS format or vice versa

For example:
T300_Slave_SP "Status as single bit"

    source IEC104_Meas 2:MSP

    destination formula T300_Slave_DP
T300_Slave_DP "Status as double bit"

   source formula SPS2DPS(T300_Slave_SP)

   destination IEC104_slave 161:MDP

See User Manual – Easergy Builder section 6

Reply
John_Archer1
Ensign John_Archer1
Ensign

Posted: ‎2024-07-04 10:41 PM

0 Likes
1
1565
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
‎2024-07-04 10:41 PM

Thanks for the reply
But I can't write this operation, how many pages can I read in the Usermanual?
Also, should I write the formula using your example?

Reply
TomBerry
Lieutenant JG TomBerry Lieutenant JG
Lieutenant JG

Posted: ‎2024-07-08 06:01 AM

0 Likes
0
1524
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
‎2024-07-08 06:01 AM

The list of data point types supported by 104 are described in section 1.3.3 of the 104 User Manual.

The Mxxx point types are only used with the Status or Analog variables. The information travels in 'monitor direction' (from the controlled station to the controlling station). 

The Cxxx point types are only used with the Command or Setpoint variables. The information travels in 'control direction' (from the controlling station to the controlled station).

 

For example

A single bit information received from device 1 would be defined in the Status data table, and have a source coordinate like xxx.MSP

Double bit information sent to device 2 would be defined in the Command data table, with a destination coordinate like yyy.CDC

 

Reply
Rajasekar_Chandrasekar
Ensign Rajasekar_Chandrasekar Ensign
Ensign

Posted: ‎2024-09-25 12:10 AM

0 Likes
1
1319
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
‎2024-09-25 12:10 AM

@John_Archer1  Please refer to the below example how to read the MSP then MSP to MDP, 

Rajasekar_Chandrasekar_0-1727248097731.png

I hope this will help solve your Problem.

BR

Rajasekar

Reply
John_Archer1
Ensign John_Archer1
Ensign

Posted: ‎2024-09-25 05:57 AM

0 Likes
0
1298
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
‎2024-09-25 05:57 AM

Thanks, I'll try it and let you know

Reply
Preview Exit Preview

never-displayed

You must be signed in to add attachments

never-displayed
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.