Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

PowerLogic™ P5 (Easergy P5) PTP & RSTP

Protection & Control

Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
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
  • EcoStruxure Power & Grid
  • Protection & Control
  • PowerLogic™ P5 (Easergy P5) PTP & RSTP
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Araceli_Monje
Commander Araceli_Monje Commander
43
Arun-kumar_PS
Commander Arun-kumar_PS Commander
21
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Related Products
product field
PowerLogic
PowerLogic P3

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Protection & Control
Start a Topic
Solved
Ivan_Puškaš_EC
Lieutenant Ivan_Puškaš_EC
Lieutenant

Posted: ‎2024-01-22 02:02 AM

0 Likes
3
1662
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
‎2024-01-22 02:02 AM

PowerLogic™ P5 (Easergy P5) PTP & RSTP

Hi,

 

End user has a request to use PTP time synchronization and the communication architecture should be RSTP ring for IEC61850 protocol.

 

As per manual for the PowerLogic™ P5 PTP is only available with HSR/PRP module on slots MN. 

There is also possibility to have RSTP card on slot L on the same relay. At least in the order form.

 

Here are some questions that came in mind:

1. Can HSR/PRP and RSTP card be on the same relay?

2. If PTP is only available with HSR/PRP card, does this means that the PTP time synchronization clock should be connected to this ring on slot NM? or PTP can be provided trough RSTP (slot L) ethernet ports?

3. Is there a way to have RSTP and PTP simultaneously?

 

Thanks for the answers.

 

Bets regards,

 

  • Thumbnail of PowerLogic P3
    PowerLogic
    PowerLogic P3
View products (1)
Labels
  • Labels:
  • IEC61850
  • PowerLogic P5
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Ivan_Puškaš_EC
Lieutenant Ivan_Puškaš_EC
Lieutenant

Posted: ‎2024-03-05 12:32 AM

0 Likes
0
1567
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
‎2024-03-05 12:32 AM

Thanks for replay.

 

"But why not use PRP or HSR , these two protocols are all redundancy protocol, more stable than RSTP. "

I agree, but it was the tender specification. Unfortunately technical aspect of the request is pointless, but other vendors have that implemented (PTP+RSTP) so we needed to choose two cards to have a valid offer.

 

BR,

See Answer In Context

Reply
Replies 3
Chunmei_Yang
Lieutenant JG Chunmei_Yang Lieutenant JG
Lieutenant JG

Posted: ‎2024-01-25 06:35 PM

1 Like
1
1636
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
‎2024-01-25 06:35 PM

Dear colleague:

Kindly find my comments in blue regarding you question.

1. Can HSR/PRP and RSTP card be on the same relay?

You can select HSR/PRP board and one ethernet card(with RSTP) at slot L for P5X30, but it not a case for P5X20 as no slot L available for P5X20.

2. If PTP is only available with HSR/PRP card, does this means that the PTP time synchronization clock should be connected to this ring on slot NM? or PTP can be provided trough RSTP (slot L) ethernet ports?

Currently for P5 product, Only PRP/HSR board support PTP time synchronization.  RSTP mode not supported.

3. Is there a way to have RSTP and PTP simultaneously?

I think it need to select PRP/HSR board for PTP and another ethernet board at slot L for RSTP.

But why not use PRP or HSR , these two protocols are all redundancy protocol, more stable than RSTP. 

 

Hope these can answer your question.

Chunmei

Reply
Ivan_Puškaš_EC
Lieutenant Ivan_Puškaš_EC
Lieutenant

Posted: ‎2024-03-05 12:32 AM

0 Likes
0
1568
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
‎2024-03-05 12:32 AM

Thanks for replay.

 

"But why not use PRP or HSR , these two protocols are all redundancy protocol, more stable than RSTP. "

I agree, but it was the tender specification. Unfortunately technical aspect of the request is pointless, but other vendors have that implemented (PTP+RSTP) so we needed to choose two cards to have a valid offer.

 

BR,

Reply
jinliu
jinliu Cadet
Cadet

Posted: ‎2025-05-29 01:42 AM

0 Likes
0
822
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
‎2025-05-29 01:42 AM

on the P5, only HSR/HSR board support PTP
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.