Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
This forum is created for the exchange of information and open dialogue regarding electrical power monitoring and energy automation products and services. Participants will have access to downloadable material as well as chat opportunities with subject matter experts.
Search in
Posted: 2021-02-25 12:37 PM . Last Modified: 2021-02-25 12:41 PM
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-02-25 12:37 PM . Last Modified: 2021-02-25 12:41 PM
When updating my SAGE RTU to the latest firmware version, when do I need to use the initial installer and config converter programs?
@Anonymous user
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-02-25 01:18 PM . Last Modified: 2021-04-08 04:37 PM
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-02-25 01:18 PM . Last Modified: 2021-04-08 04:37 PM
INITIAL INSTALLER
The Initial Installer utility is only used when converting an existing, "red CPU" card based SAGE RTU running non-secure firmware to the Secure Firmware, (J0 and beyond - current Rev is C3414-500-S02K5_P2).
The utility updates the existing configuration in place on the compact flash, but also modifies the directory structure on the Compact Flash to that needed by the secure firmware.
Initial Installer utility only needs to be performed once.
CONFIG CONVERTER
If you download a secure firmware update package (J0 or later) from the sage-rtu.com website, it comes with a Config Converter that will update an existing secure firmware configuration from an earlier revision to the firmware update package revision. It is located in the Update/Secure/updateGen folder.
However, there is a multi-step process required to convert a non-secure configuration to secure, depending on the hardware it is from, either 2200 or 2300/2400 (both non-secure).
2300 and 2400 non-secure to Secure Firmware config (offline version):
All non-secure firmware configuration must be at the G3 revision for any Secure Firmware Config Converter to be able to convert it properly. You can download the G3 Firmware Update package to obtain the G3 Config Converter utility. Once your configuration is converted to G3, the Secure Firmware Config converter can import it and create the equivalent secure firmware configuration package to be uploaded directly to the RTU.
2200 config to Secure Firmware:
Convert to B6, using the config converter supplied with the secure firmware package. (Update/Secure/config_converters/S2200/Convert_to_B6_1.6.exe)
Convert the B6 config to G3, using the config converter supplied with the (Update//Secure/config_converters/C3414/Convert_to_G3_6.4.exe)
Finally, use the secure config converter to create the secure config (Update/Secure/updateGen/Config_Converter_K5.exe)
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-02-25 01:18 PM . Last Modified: 2021-04-08 04:37 PM
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-02-25 01:18 PM . Last Modified: 2021-04-08 04:37 PM
INITIAL INSTALLER
The Initial Installer utility is only used when converting an existing, "red CPU" card based SAGE RTU running non-secure firmware to the Secure Firmware, (J0 and beyond - current Rev is C3414-500-S02K5_P2).
The utility updates the existing configuration in place on the compact flash, but also modifies the directory structure on the Compact Flash to that needed by the secure firmware.
Initial Installer utility only needs to be performed once.
CONFIG CONVERTER
If you download a secure firmware update package (J0 or later) from the sage-rtu.com website, it comes with a Config Converter that will update an existing secure firmware configuration from an earlier revision to the firmware update package revision. It is located in the Update/Secure/updateGen folder.
However, there is a multi-step process required to convert a non-secure configuration to secure, depending on the hardware it is from, either 2200 or 2300/2400 (both non-secure).
2300 and 2400 non-secure to Secure Firmware config (offline version):
All non-secure firmware configuration must be at the G3 revision for any Secure Firmware Config Converter to be able to convert it properly. You can download the G3 Firmware Update package to obtain the G3 Config Converter utility. Once your configuration is converted to G3, the Secure Firmware Config converter can import it and create the equivalent secure firmware configuration package to be uploaded directly to the RTU.
2200 config to Secure Firmware:
Convert to B6, using the config converter supplied with the secure firmware package. (Update/Secure/config_converters/S2200/Convert_to_B6_1.6.exe)
Convert the B6 config to G3, using the config converter supplied with the (Update//Secure/config_converters/C3414/Convert_to_G3_6.4.exe)
Finally, use the secure config converter to create the secure config (Update/Secure/updateGen/Config_Converter_K5.exe)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-04-09 02:09 PM
We recently held a webinar which goes in depth on this topic, including how to perform config updates when performing CPU upgrades from SAGE 2200, SAGE 2300 to the latest secure firmware.
We also covered converting from non-secure 2400's to the latest firmware as well as secure to secure configuration updates.
You can watch the session here under the 2021 -> Week 3 folder.
I hope that helps to clarify when and how to migrate from any previous CPU to the latest firmware to take advantage of the cool features we have implemented recently (an explanation also included in the webinar).
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.