Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84601members
353871posts

Standard for Heat Tag

Power Distribution and Digital

Join experts & peers to learn, share and engage about the key trends of electrical distribution around safety, availability, efficiency and connectivity, as well as power standards & regulations. From design to implementation and operation, let’s discuss how digital and software are transforming your business and your day-to-day work.

Solved
Widiyatmoko
Ensign
Ensign

Standard for Heat Tag

As Schneider now already have Heat Tag then which standard Schneider use ? How we can make it in technical specification for tender ? Is this standard align with SNI, if yes then which SNI apply for this.

@HelvinHermanT @Widiyatmoko @reinierliman 

 

Thanks,

Tags (1)

Accepted Solutions
Kiran_Lagwankar
Ensign Ensign
Ensign

Re: Standard for Heat Tag

The Heat Tag SMART sensor complies with :

 

IEC 61010-1:2017 UL/CSA/EU CENELEC deviations

 

IEC/EN 61326-1b FCC Part 15B and 15C

 

ETSI/EN 300328

 

ETSI/EN 301489-1

 

IEEE 802.15.4

See Answer In Context

Tags (1)
1 Reply 1
Kiran_Lagwankar
Ensign Ensign
Ensign

Re: Standard for Heat Tag

The Heat Tag SMART sensor complies with :

 

IEC 61010-1:2017 UL/CSA/EU CENELEC deviations

 

IEC/EN 61326-1b FCC Part 15B and 15C

 

ETSI/EN 300328

 

ETSI/EN 301489-1

 

IEEE 802.15.4

Tags (1)