The latest version of the Ecodial application is working in 6 languages. They are English, French, Spanish, Turkish, Portugese and Russian.
So, we can change and generate the "project report" in different language than the language of the application.
Let us see,
How to select and change the different language for the "Project Report.”
Step 1:
Draw the electrical network as per the requirement and calculate the project.
Step 2 :
After the successful calculation, kindly switch to “Report” tab...Then the application will automatically generate report in default language.
Step 3 :
We can see at the Left-hand side, there is an option to change the "Report language."

Step 4 :
Change the language (ex. Turkish) and click on the Generate button. The project report will be generated for the selected language.