Pod sharing
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
  • EcoStruxure IT Help Center
  • EcoStruxure IT Help Center Categories
  • Data Center Expert
  • Monitoring NetBotz Appliances in DCE
  • Pod sharing
Options
  • My Knowledge Base Contributions
  • Subscribe
  • Bookmark
  • Invite a Friend
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • EcoStruxure IT Forum

  • APC UPS Data Center & Enterprise Solutions Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite

EcoStruxure IT Support

Submit a support request for additional assistance with EcoStruxure IT software.

Request Support

Pod sharing

Sort by:
Helpfulness
  • Date
  • Views
  • Likes
  • Comments
  • Helpfulness
Options
  • Subscribe
  • Bookmark
  • Invite a Friend

Update Remote Device display

  Configure the settings used for HTTP or HTTPS communication between the pod-sharing host and the remote devices. Element Description Host/IP Address Identify the hostname or IP address of the remote device that has pods you want it to share with the host NetBotz Appliance. Port Identify the port used for the communication: default is 80 for HTTP, and 443 for HTTPS. SSL Options Select how the Secure Sockets Layer (SSL) protocol will be used for the communication with the remote device: None, Require SSL - No verification, Require SSL - Verify certificate, or Require SSL - Verify certificate and hostname. User ID Type in the User ID to be used to access the remote device. Note Some remote pod functionality may be unavailable if the user ID is for a user account that does not have Administrator privileges. Password Type in the password to be used with the User ID to access the remote device. Confirm Password Retype the password. Timeout (seconds) Define how long, in seconds, the host NetBotz Appliance will wait for a response before it considers an attempt to communicate with a remote device has failed.  
View full article
Picard EcoStruxureIT
‎2019-11-20 06:13 AM

424 Views

Pod sharing overview

    Pod sharing overview Pod Sharing enables your NetBotz 500 or 550 Appliance to connect with, and receive data directly from, pod devices integrated with or connected to NetBotz Appliances, certain Pelco cameras, and AP9361 APC NetBotz Rack Access devices. These shared pods can be an integrated camera or sensor pod, or externally connected pods. With pod Sharing, a single NetBotz 500 or 550 Appliance acts as a facility host to manage alerts from many other NetBotz Appliances, certain Pelco cameras, and AP9361 APC NetBotz Rack Access devices, distributed throughout your network. Once a pod is shared with the host NetBotz 500 or 550 Appliance, it functions as though it were connected directly to that NetBotz appliance. A single NetBotz 500 can host up to 16 shared pods, total. Up to 4 of the shared pods can be Camera Pod 120s or CCTV Adapter pods. The shared pods can be physically connected to up to 8 target devices. A NetBotz 500 or 550 host can share pods with RackBotz and WallBotz 320, 350, 420, 450, 500, and 550 NetBotz Appliances, as well as with legacy NetBotz devices that run BotzWare 1.x (including RackBotz and WallBotz 300, 303, 310, 400, and 410 devices). Once a NetBotz 500 is configured to access these legacy models they are treated exactly like other shared pods or devices, providing alert and sensor data exactly as if they were directly connected to the NetBotz 500. It is important to note the following concerning pod sharing. The Pod Sharing task can be run only on one device at a time. A NetBotz 500 v2.6 or later, or a NetBotz 550, can host remote pods without using the optional Premium Software Module that must be used with earlier NetBotz 500 versions for pod sharing. Pods that are not physically connected to a device do not count against the total number of USB-connected devices allowed for the NetBotz Appliance model. A NetBotz 420 supports an additional camera pod and up to four additional non-camera pods. A NetBotz 500 or 550 supports up to four camera pods and up to 17 non-camera pods. Frame rate from remotely hosted camera pods is limited to 10 frames per second. The camera image resolution available from a hosted camera pod is determined by the maximum resolution available to the device to which the pod is physically connected. For example, for a Camera Pod 120 connected to a NetBotz 500, the maximum resolution is 1280x1024. However, if the Camera Pod 120 is connected to a NetBotz 420, the maximum is 640x480.
View full article
Picard EcoStruxureIT
‎2019-11-20 06:14 AM

683 Views

Pod Sharing Settings option

    Pod Sharing Settings option Use this option's configuration display to configure a selected NetBotz 500 or 550 Appliance to host virtual pods for remote NetBotz Appliances, certain Pelco cameras, and AP9361 APC NetBotz Rack Access PX - HID devices. Element Description Remote Devices Identify the remote devices you want to have share their pods with a selected NetBotz 500 or 550 Appliance by using the "Update Remote Device" display to add a new remote device, or edit or delete an existing one. Shared Pods With a remote device selected in the Remote Devices list, highlight one or more of its pods in this Shared Pods list. Then click Share Remote Pod, to share the selected pods with the NetBotz 500 or 550 host, or Stop Sharing Pod, to stop sharing those pods. Note The NetBotz Appliance entry allows you to select whether you want to share the integrated pods at that appliance.  
View full article
Picard EcoStruxureIT
‎2019-11-20 06:14 AM

486 Views
Didn't find what you are looking for? Ask our Experts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.