Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Quantum Modernization to M580

Modicon PAC Forum

A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.
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
  • Industrial Automation
  • Modicon PAC Forum
  • Re: Quantum Modernization to M580
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Trinxs1
Trinxs1 Leader
19
YONGHO-KIM
YONGHO-KIM Mentor
10
ciupol
ciupol
9
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Modicon PAC Forum
Start a Topic
Solved
Rifqi_Imanto
Rifqi_Imanto Troubleshooter
Troubleshooter

Posted: ‎2020-03-29 10:32 PM

0 Likes
4
8305
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
Posted: ‎2020-03-29 10:32 PM

Quantum Modernization to M580

Hi,

 

is it possible to to replace Quantum 140 CPU 43412U to M580 BME P58 1020 ? with all module replaced, and with minimal risk and modification.

 

image.png

 

and what possibility issue will appear? 

  1. State Ram Addressing (Quantum Start from 1, and M580 start from 0) will make some Real/Float type data error. and how to fix it?
  2. Re-Addressing on SCADA (Citect SCADA) side? (User doesn't want to do this)
  3. anything else?

 

Thanks

@Anonymous user 

Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
RoozeeR
RoozeeR Mentor
Mentor

Posted: ‎2020-03-29 11:57 PM

3 Likes
2
8302
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
Posted: ‎2020-03-29 11:57 PM

Hi,

1 & 2. Re-adressing is not needed when  %SW138 - %SW141 are set with an initial value of 1. These Status words are available for M580 and give the STATE-RAM addresses an offset (of 1), making all STATERAM addresses identical as in your Quantum application. No need to change your SCADA application for this.

Unity M580 Application Converter (UMAC) is the tool for conversion of Quantum/Premium to M580 and will set these values automatically.

 

Also UMAC will add some code to make 32-bit variables (float, DINT), compatible with M580, without impacting your SCAD application.

 

3. Check connections on the CPU. 140CPU43412 has 2 Modbus ports and MB+, they do not show on this bitmap, but devices might be connected. For Modbus connection add a BMXNOM0200 (Check cables) and for MB+ add a MB+ Proxy module.

 

Conversion cabling for the IO modules is available, making the IO conversion more easy.

R.Roozee
Sr Solution Architect (SAE Master)

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Replies 4
RoozeeR
RoozeeR Mentor
Mentor

Posted: ‎2020-03-29 11:57 PM

3 Likes
2
8302
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
Posted: ‎2020-03-29 11:57 PM

Hi,

1 & 2. Re-adressing is not needed when  %SW138 - %SW141 are set with an initial value of 1. These Status words are available for M580 and give the STATE-RAM addresses an offset (of 1), making all STATERAM addresses identical as in your Quantum application. No need to change your SCADA application for this.

Unity M580 Application Converter (UMAC) is the tool for conversion of Quantum/Premium to M580 and will set these values automatically.

 

Also UMAC will add some code to make 32-bit variables (float, DINT), compatible with M580, without impacting your SCAD application.

 

3. Check connections on the CPU. 140CPU43412 has 2 Modbus ports and MB+, they do not show on this bitmap, but devices might be connected. For Modbus connection add a BMXNOM0200 (Check cables) and for MB+ add a MB+ Proxy module.

 

Conversion cabling for the IO modules is available, making the IO conversion more easy.

R.Roozee
Sr Solution Architect (SAE Master)
Reply

Link copied. Please paste this link to share this article on your social media post.

Rifqi_Imanto
Rifqi_Imanto Troubleshooter
Troubleshooter

Posted: ‎2020-03-30 12:35 AM

In response to RoozeeR
1 Like
0
8300
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
Posted: ‎2020-03-30 12:35 AM

@RoozeeR 

 

ok nice..

for point 3. there is only IO, no communication bus to field. 

 

Thanks

Reply

Link copied. Please paste this link to share this article on your social media post.

Anonymous user
Not applicable

Posted: ‎2020-09-29 06:25 AM

0 Likes
0
8255
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
Posted: ‎2020-09-29 06:25 AM

Hello 

 

You need to have minimum the Level 4 M580 - BMEP584040 to support Quantum migration and integrate M580 rack with existing Quantum IO.

 

Also, Schneider has an internal tool to migrate existing Quantum program to M580 program without having to mess PLC addressing offsets and keeping SCADA addressing intact.  Please discuss with your local SE sales person 

  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

Archie.Levivi22
Archie.Levivi22
Explorer

Posted: ‎2024-10-23 06:33 AM

In response to RoozeeR
0 Likes
0
3562
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
Posted: ‎2024-10-23 06:33 AM

Hi 

 

Do you have a part number for this "Conversion cabling for the IO modules is available, making the IO conversion more easy." Cable?
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.