Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

M580 communication with HMIGXU5512 is working only in CPU service port, why ?

Modicon PAC Forum

A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.
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
  • Industrial Automation
  • Modicon PAC Forum
  • M580 communication with HMIGXU5512 is working only in CPU service port, why ?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Trinxs1
Trinxs1 Leader
19
YONGHO-KIM
YONGHO-KIM Mentor
10
ciupol
ciupol
9
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Related Products
product field
Schneider Electric
EcoStruxure™ Control Expert

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Modicon PAC Forum
Start a Topic
Solved
ArunrajPremraj
ArunrajPremraj Contributor
Contributor

Posted: ‎2022-03-11 02:02 AM

0 Likes
2
3309
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
Posted: ‎2022-03-11 02:02 AM

M580 communication with HMIGXU5512 is working only in CPU service port, why ?

Hi,

 

I am trying to establish a communication with HMI using ETH- 1 and ETH-2 ports or the M580 CPU ,  But HMI is not gives " plc communication failed " error. 

 

But when i connect it to CPU service port it works,  I tried port mirroring also. .still not working. 

 

i dont want to use Service port for communication purpose. 

 

i have a switch connected to ETH-1 port and the HMI and other devices are communicating via the switch. 

 

HMI communication works only if i connect to CPU Service port. 

 

I have checked the ETH-1 and ETH-2 ports. both are healthy and can upload and download , ping IP's and are healthy. .. 

 

what is the issue here..?   

 

 

thanks.

Labels
  • Labels:
  • 01. Modicon M340 PAC
  • 02. Modicon M580 ePAC
  • 06. EcoStruxure Control Expert
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
DenisGoyette
DenisGoyette Contributor
Contributor

Posted: ‎2022-03-11 05:48 AM

0 Likes
1
3291
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
Posted: ‎2022-03-11 05:48 AM

Hi,

 

What model of M580 CPU is this? If it's a xx40 model, ie. BMEP582040, I remember seeing that the 2 bottom ports are used (reserved) for the ERIO architecture. Other type of traffic will not get through (unless using specific cards or connexium switches). You would have the same behavior if you would try to do modbus TCP/IP IO scanning out of those 2 ports.

 

You do not get that behavior out of the xx20 models, since they do not support ERIO.

 

So you'll need to use the service port of the cpu to connect your HMI, or add a BMENOC card to your setup.

 

I can't find the documentation explaining that at the moment unfortunately.

See Answer In Context

  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

Replies 2
DenisGoyette
DenisGoyette Contributor
Contributor

Posted: ‎2022-03-11 05:48 AM

0 Likes
1
3292
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
Posted: ‎2022-03-11 05:48 AM

Hi,

 

What model of M580 CPU is this? If it's a xx40 model, ie. BMEP582040, I remember seeing that the 2 bottom ports are used (reserved) for the ERIO architecture. Other type of traffic will not get through (unless using specific cards or connexium switches). You would have the same behavior if you would try to do modbus TCP/IP IO scanning out of those 2 ports.

 

You do not get that behavior out of the xx20 models, since they do not support ERIO.

 

So you'll need to use the service port of the cpu to connect your HMI, or add a BMENOC card to your setup.

 

I can't find the documentation explaining that at the moment unfortunately.

  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

ArunrajPremraj
ArunrajPremraj Contributor
Contributor

Posted: ‎2022-03-13 09:31 PM

In response to DenisGoyette
0 Likes
0
3229
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
Posted: ‎2022-03-13 09:31 PM

Thank you very much for the reply,  I am using BMEP582040 exactly.  I will try to use a connexium switch and see if it works.  I possible can u guide me or direct me on how to configure Connexium Switch ports to connect to HMI?

 

Thanks in advance!!!
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.