A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2024-06-1410:39 AM
M340 Ethernet Connection Problem
I have configured my Ethernet Network connectio (called Ethernet_1) and have linked it to Ethernet Channel 3 on the M340 PLC. I've set it to use ETH TCP IP.
When I Set the Address in Control Expert I select MODBUS TCP and then go to communication parameters / driver settings. From there I can select Modbus test, enter the IP address of the PLC and it connects. When I click start I get lots of activity on my network switch.
The problem is when I try to go online from Control Expert using the MODBUS TCP:SYS connection. I get the following: