Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84424members
353614posts

Control Expert Windows within windows

Modicon PAC Forum

A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.

Trinxs1
Lieutenant Lieutenant
Lieutenant

Control Expert Windows within windows

Control Expert please remove small Windows within large windows

 

There is a need to remove nuisance windows within Control expert. 

 

For example with the configuration of the BMENOC0301 module there is a "Switch" tab which displays a large window but then places a smaller window for the configuration of the four ports of the BMENOC module i.e. Service port, control ports and backplane port.  The issue is that this window displays 3 items and you must scroll down for the fourth port which is often the most likely one you need to check or modify.

 

Please refer to the attached image.

Trinxs
Senior Technical Sales Consultant - PAC
Attachments
1 Reply 1
JerryBartlemay
Ensign Ensign
Ensign
0 Likes
0
827

Re: Control Expert Windows within windows

I agree with the concept, but don't have a problem with the small window.  It should be made large enough to view everything within the space available though.