Enhance Modbus device DTM to support other Modbus Function codes then 3,16 & 23

Modicon Ideas & new features

Have ideas on how to improve Modicon? Please share and get votes from Community to influence development efforts.
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
  • Industrial Automation
  • Modicon Ideas & new features
  • Enhance Modbus device DTM to support other Modbus Function codes then 3,16 & 23
Options
  • Mark as New
  • Mark as Read
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Top Labels
  • Alphabetical
  • 06. EcoStruxure Control Expert 44
  • 02. Modicon M580 ePAC 21
  • 05. Networking & Communication 11
  • 01. Modicon M340 PAC 8
  • 03. Modicon PAC Safety 3
  • 04. Modicon X80 IO 3
  • 12. Other 2
  • 08. Tools & Resources 1
  • 07. Modicon PAC Legacy 1
  • 09. Surveys 1
  • 10. Australia 1
Idea Statuses
  • Submitted 48
  • Needs more info 0
  • Under consideration 2
  • Accepted 2
  • Declined 0
  • To be deleted 0
  • Delivered 3
Related Products
Thumbnail of Modicon M580
Schneider Electric
Modicon M580
7
Thumbnail of EcoStruxure™ Control Expert
Schneider Electric
EcoStruxure™ Control Expert
6
Thumbnail of Modicon M340
Schneider Electric
Modicon M340
2
Load more
Completed Ideas
  • EcoStruxure Control Expert - DTM Update Tool

  • The ability to access DTMs in a different subnet via the DTM browser

  • [networks] Should we implement PRP in our network offer?

View All
Top Liked Authors
User Likes Count
Snacky
Ensign Snacky
1
View All

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
25 Likes

Enhance Modbus device DTM to support other Modbus Function codes then 3,16 & 23

Status: Under consideration Submitted by Lt. Commander RoozeeR Lt. Commander on ‎2020-11-09 12:32 AM
7 Comments (7 New)

Modicon/Schneider Electric are the founders of Modbus and Modbus/TCP. However in our software we limit the users in functionality. All years I'm with the company, this questions pops-up regularly:

Why does Schneider NOT support the use of other Modbus function codes than 3, 16 and 23 in IO-scanning?

Other function codes can be implemented (read of %IW/3xxxx references) using DATA-EXCH functions, which is a lot of programming effort and introduces limitations, IO-scanning doesn't have.

Today I got a question (again) from one of our alliance partners: Why does Schneider not support other Modbus function codes than 3,16 and 23 while competitors like Mitsubishi, Phoenix Contact and WAGO offer this functionality by default?

Can't the Modbus Device DTM be enhanced to offer this functionality?

Tags (1)
  • Find more ideas tagged with:
  • english
Labels (4)
See more ideas labeled with:
  • 01. Modicon M340 PAC
  • 02. Modicon M580 ePAC
  • 05. Networking & Communication
  • 06. EcoStruxure Control Expert
Comment

Link copied. Please paste this link to share this article on your social media post.

  • Back to Idea Exchange
  • Previous
  • Next
7 Comments
SEStig
Ensign SEStig Ensign
Ensign
‎2022-02-24 04:54 PM
  • Mark as Read
  • Mark as New
  • Bookmark
  • Permalink
  • Print
  • Email to a Friend
  • Report Inappropriate Content
‎2022-02-24 04:54 PM

If extra function codes are what you want then the actual "DTM" for a modbus device should be completely revamped.

 

Currently it isn't what i would call a DTM because there are actually no configuration options when you open it in the DTM browser. It merely provides a way for the CPU/NOC etc to instantiate a device that will use modbus functions which you need to define in the CPU/NOC rather than the device itself. This leads to the issue of not being able to copy/paste modbus devices once set up.

 

In the modbus device dtm you should be able to specify function codes, rep rates or trigger types etc which then GENERATES the modbus table in the NOC/CPU in the same way a VSD DTM does.

 

The best example of how this should be implemented is in the Generic Modbus device in EcoStruxure Machine Expert. This has all the above functions and can be duplicated once a device has been set up correctly.

 

Ideally you would be able to create a new device using the Modbus DTM, configure it with all the required reads/writes/data types etc then save it to a custom library for later reuse on another project.

Trinxs1
Lt. Commander Trinxs1 Lt. Commander
Lt. Commander
‎2023-03-09 03:32 AM
  • Mark as Read
  • Mark as New
  • Bookmark
  • Permalink
  • Print
  • Email to a Friend
  • Report Inappropriate Content
‎2023-03-09 03:32 AM
Status changed to: Under consideration

This feature of has been included in the product backlog.    It has not been assigned to any version yet.

Patrick_Nijenhuis
Patrick_Nijenhuis
Cadet
‎2023-06-12 06:19 AM
  • Mark as Read
  • Mark as New
  • Bookmark
  • Permalink
  • Print
  • Email to a Friend
  • Report Inappropriate Content
‎2023-06-12 06:19 AM

Good point from Rene Rozee

We have the problem now that we have to read input registers and coils. The current DTM does not support that and that is strange because the Modbus protocol and the DTM are both from Schneider, can't be that hard to implement this in the DTM.

dnordenberg1
Lt. Commander dnordenberg1
Lt. Commander
‎2023-10-11 07:05 AM
  • Mark as Read
  • Mark as New
  • Bookmark
  • Permalink
  • Print
  • Email to a Friend
  • Report Inappropriate Content
‎2023-10-11 07:05 AM

I think schneider wanted to forget about these old and less used modbus telegrams because everything fits in a standard holding register which is what modern remote IOs use for both digital and analog values today. But sometimes you still come across exotic devices that still uses them and it's a bit annoying that you have to handle them in completely different way then 😞 So I totally agree with this feature request.

ciupol
Lt. Commander ciupol
Lt. Commander
‎2023-10-12 06:09 AM
  • Mark as Read
  • Mark as New
  • Bookmark
  • Permalink
  • Print
  • Email to a Friend
  • Report Inappropriate Content
‎2023-10-12 06:09 AM

I do not think that it is only exotic devices. I have a lot of modern devices that still use registers other than 4x.

Patrick_Nijenhuis
Patrick_Nijenhuis
Cadet
‎2023-10-13 03:01 AM
  • Mark as Read
  • Mark as New
  • Bookmark
  • Permalink
  • Print
  • Email to a Friend
  • Report Inappropriate Content
‎2023-10-13 03:01 AM

I agree with that, I saw mere then once that other commands are beiing used and now is is a lot of work for something that should be in de DTM. When it can be configured in the DTM then all communication outside of the PLC is done from one point. Now you have to go through the software to find all communication connections.

ciupol
Lt. Commander ciupol
Lt. Commander
‎2023-10-25 06:08 AM
  • Mark as Read
  • Mark as New
  • Bookmark
  • Permalink
  • Print
  • Email to a Friend
  • Report Inappropriate Content
‎2023-10-25 06:08 AM

If this will ever be implemented it should allow to select particular modbus command user wants to use. For example I run into devices that support only function code 06 (write single register) or only function code 16 (write multiple registers). With the device that uses only function code 06 I was not even able to use the WRITE_VAR block (or IO scanner or anything else) as it uses code 16. I had use use DATA_EXCH block and construct my own custom modbus requests which is obviously quite cumbersome.

Comment
Preview Exit Preview

never-displayed

Hint:
@ links to members, content
 
  • Back to Idea Exchange
  • Previous
  • Next
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.