Have ideas on how to improve Modicon? Please share and get votes from Community to influence development efforts.
Search in
When you add custom EDS files to your project you have to add them to Control Expert on any workstation that you will work on with the project. The idea is to include custom EDS files that are use in the project into project file (STU) so that they can be automatically added when project is open on workstation without those EDS files added. There may be a pop-up during opening the project asking if user wants to add those EDS files. Also there may be a setting in project settings allowing user to select if he/she want to add EDS files to project file.
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.