Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

trying to set up a modbus export module in a VIP to send data to an ION meter

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • trying to set up a modbus export module in a VIP to send data to an ION meter
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
195
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
james_bougie_gp
james_bougie_gp
Explorer

Posted: ‎2020-05-15 09:53 AM

2 Likes
4
3294
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
‎2020-05-15 09:53 AM

trying to set up a modbus export module in a VIP to send data to an ION meter

We are trying to move data from a VIP to a BMS system.  We would like ti use modbus to do this and was thinking about using an ION meter to do this.

 

Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2020-05-16 03:24 PM

2 Likes
3
3285
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
‎2020-05-16 03:24 PM

Hello @james_bougie_gp 

 

To have VIP write a value to an ION meter, the easiest way to do this is with a Distributed numeric module on VIP linked to External numeric on the ION meter. Then have External number linked to desired modbus slave module. The distributed numeric modules do have default modbus maps if you would prefer to use those.

 

On A side note, with PME 2020, I believe the VIP can now be configured as a modbus TCP slave. 

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2020-05-27 09:52 AM

2 Likes
1
3266
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
‎2020-05-27 09:52 AM

Hello,

 

In management console, you can setup device security. I would make sure the user setup there is correct.

 

Charles

 

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Replies 4
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2020-05-16 03:24 PM

2 Likes
3
3286
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
‎2020-05-16 03:24 PM

Hello @james_bougie_gp 

 

To have VIP write a value to an ION meter, the easiest way to do this is with a Distributed numeric module on VIP linked to External numeric on the ION meter. Then have External number linked to desired modbus slave module. The distributed numeric modules do have default modbus maps if you would prefer to use those.

 

On A side note, with PME 2020, I believe the VIP can now be configured as a modbus TCP slave. 

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
dmcGPT
dmcGPT
Explorer

Posted: ‎2020-05-26 07:24 PM

0 Likes
2
3270
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
‎2020-05-26 07:24 PM

Hello @Charles_Murison and @james_bougie_gp 

In PME 9.0, I set this up and received the following error in the "Event" Output registers of the Distributed numeric module: "Write Failed - Insufficient security to perform Distributed Control Operation"
I may need to modify something on the Data Monitor module, Distributed Numeric module or the External Numeric module or a meter or VIP security setting...
Please see screenshots below for more information. Any and all help is much appreciated!

Dist Num 1 Config.JPGDist Num 1 Input.JPGDist Num 1 Output.JPGEN4 Output.JPGMeter Security Settings.JPG

 

The outputs below are:
1) Value (31) from Arithmetic module generated in the meter.
2) Value from Ext Num 4, which is linked from the VIP, arithmetic module 
3) Value from Ext Num 5, which is linked from the VIP, counter module

Modbus slave inputs.JPGOverall.JPG

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2020-05-27 09:52 AM

2 Likes
1
3267
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
‎2020-05-27 09:52 AM

Hello,

 

In management console, you can setup device security. I would make sure the user setup there is correct.

 

Charles

 

L4 Prime for Advanced metering and Utilities
Reply
dmcGPT
dmcGPT
Explorer

Posted: ‎2020-05-28 07:07 AM

1 Like
0
3263
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
‎2020-05-28 07:07 AM

I was able to resolve the write fail by:
1) In Designer, setting the Data Monitor Module source input to be the external numeric module on the meter
Data Monitor module Source.JPG
2) As you advised, in Management Console, setting up the security settings for the meter to default user, standard security and matching the password to the meter's password
Match password.JPG
3) Restarting the VIP service
4) Disabling the meter connection in management console for a minute and then enabling it
 
Thank you for your patience in helping me resolve this issue!
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.