Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Wireless energy metering devices EM4300 series & WT4200 series

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • Wireless energy metering devices EM4300 series & WT4200 series
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
581
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
Anonymous user
Not applicable

Posted: ‎2015-08-31 03:57 PM

1 Like
0
1035
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
‎2015-08-31 03:57 PM

Wireless energy metering devices EM4300 series & WT4200 series

Eagle project passed Sell gate for Europe last week (wk34). Sell gate for USA is planned for mid to late Q4 2015.

is Program Manager for the Retrofit V2 program, which consists of the Condor project (EM4300 series) and the Eagle project (WT4100 series / WT4200 series). Both projects deliver products targeted for existing buildings (#brownfield  applications).

The EM4300 series 3-phase energy meter features a compact DIN rail-mount form factor, ZigBee Pro wireless communications and  Rogowski coil current sensors (200, 500, 1000 or 2000 A rated current options).

WT4100 / WT4200 series devices use long-range RF wireless communications to deliver WAGES energy data. A typical installation requires one wireless receiver and one or more sensor-transmitters:

  • Sensor-transmitter device types include pulse counter, status monitor, 0-10V analog input, or ambient temperature.
  • Wireless receiver supports up to 255 sensor-transmitters. Received data is converted to Modbus RTU for use in your existing energy monitoring system.
  • Wireless repeater extends the effective transmission range up to 10 km.

Technical documentation is available on our website. Search for "EM4300 series", "WT4200 series" and "WR4200 series" for installation sheets and user guides.

Companion projects supporting the EM4300 series and WT4100 / WT4200 series devices include the Com'X 200 and Facilities Insight.

Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 0
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.