Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Swp Accusine Configuration

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • Swp Accusine Configuration
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
217
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
sesa296930_brid
sesa296930_brid Explorer
Explorer

Posted: ‎2016-02-05 04:07 AM . Last Modified: ‎2020-12-02 03:31 AM

0 Likes
3
1895
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
‎2016-02-05 04:07 AM

Swp Accusine Configuration

Dear Concerned

1- We was trying to configure SWP Accusine 30 & 60 Amps  but the first step is to enter a password , In the operation guide it seems that we have to set a password but when we try a message of wrong password appears ,So is there is a default password for the device and how we can reset the password.

2- An alarm of ( Conditioner is off ) appears on one of the two accusines what does it means ?

3- At the back of the accusine controller there is a switch for lock and unlock we did not find anything about this switch in the installation and operation guides, what is the function of this switch ?

4- without running the devices One of the accusines is showing measures for current and THDs and the other is showing **** in all the parameters  , What does this means ?

It will be so appreciated if you can support ASAP as we are in site and its a critical case to the customer.

Labels
  • Labels:
  • Power Quality
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 3
sesa190510_brid
sesa190510_brid Contributor
Contributor

Posted: ‎2016-02-08 07:25 PM

1 Like
1
1812
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
‎2016-02-08 07:25 PM

Hi Amr,

1. So is there is a default password for the device and how we can reset the password?

I know how you feel. . It was happen to me also two months back. And yes it has default password. For "configuration" password you can use 1802. Unfortunately, AFAIK, we couldn't change the default password.

2. it means the accusine is not injecting any compensation. Since you weren't make any setting yet, it is understandable.

(Hi Ravindra N KULKARNI, please correct me if I'm wrong)

3. The switch must be in unlock position during setting. I think, it was purposed to prevent somebody accidentally operating Accusine.

4. The measured current should be displayed on HMI. However, during low load, CT's couldn't detect the current.

In any system with CT, please remind this rule of thumb "The loading factor of measurement CT's should be higher than 10% of its primary rating". Less than that, the CT will operating in "knee region" and shows big error due to its non-linearity.

In your case, probably in 1st unit the CT got enough current to read, however, in 2nd unit the current is so low so it can't be detected by CT.


Example: CT with ratio 300 / 5 should be loaded by at least 30 A. Otherwise we couldn't "trust" the result.

This is not a really big deal for power measurement.. You just get wrong measurement .

But in Accusine, it will inject wrong compensation and - instead of improving THDi level - it will  worsen THDi level.

I hope it's help

Regards,

Reply
sesa14764
sesa14764 Explorer
Explorer

Posted: ‎2016-02-09 09:24 AM

0 Likes
0
1812
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
‎2016-02-09 09:24 AM

Hi Amr,

I can also strongly suggest you to call your local support for this offer (CCC or BFO case) in order to have more specific answers for this particular commissioning.

Regards

Nathalie

Reply
RavindraKulkarni
RavindraKulkarni Contributor
Contributor

Posted: ‎2016-02-09 07:13 PM

2 Likes
0
1812
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
‎2016-02-09 07:13 PM

Hi Yorga,

You are right. I have replied to Amr over email, the answers to his queries. We should always use trained & qualified service engineers to commission Accusine. If commissioning is not done properly, it can cause damage to the product.

Regards,

Ravindra
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.