Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Single ION 7650 / 8650 on 2 x Ethernet networks - 2 x separate IP addresses

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • Single ION 7650 / 8650 on 2 x Ethernet networks - 2 x separate IP addresses
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
sesa72458
sesa72458 Leader
Leader

Posted: ‎2015-03-02 06:37 PM

0 Likes
4
1914
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
‎2015-03-02 06:37 PM

Single ION 7650 / 8650 on 2 x Ethernet networks - 2 x separate IP addresses

Hi,

Is it possible for an ION7650 or 8650 to operate on 2 x Ethernet networks with 2 x separate IP addresses?

I'm almost certain the meter does not support dual comms cards, but if we get a comms card with both FX and TX ports, is it possible for two completely segregated Ethernet networks to both monitor the meter?

Regards,

Steven Yan

Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2015-03-03 11:28 AM

0 Likes
1
1850
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
‎2015-03-03 11:28 AM


Hello Yan,

The short answer is neither the 7650 nor the 8650 can support 2 seperate IP address on the same device. One option would be to use Ethernet (copper or fibre) to serial converter and connect the converter to the serial port on the meter, that way each network would have its own IP address.

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Replies 4
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2015-03-03 11:28 AM

0 Likes
1
1850
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
‎2015-03-03 11:28 AM


Hello Yan,

The short answer is neither the 7650 nor the 8650 can support 2 seperate IP address on the same device. One option would be to use Ethernet (copper or fibre) to serial converter and connect the converter to the serial port on the meter, that way each network would have its own IP address.

L4 Prime for Advanced metering and Utilities
Reply
Hal_Etheridge
Hal_Etheridge Champion
Champion

Posted: ‎2015-03-03 12:22 PM

0 Likes
1
1850
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
‎2015-03-03 12:22 PM

Alternatively use a firewall or other NAT type device to present multiple IP addresses to the outside world and convert the requests to the single IP on the protected network side.  This would also allow more authentication of the meter requests if that is a requirement (like only allowing connections from specific IP addresses).  Note that this solution is probably way more elaborate than is needed though.

Reply
sesa72458
sesa72458 Leader
Leader

Posted: ‎2015-03-03 01:41 PM

0 Likes
0
1850
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
‎2015-03-03 01:41 PM

Hi Charles,

A previous integrator had done this but unfortunately the customer complained of the slow speed on the side with serial.

But it looks like it's probably the simplest way.

Regards,

Steven Yan

Reply
sesa72458
sesa72458 Leader
Leader

Posted: ‎2015-03-03 01:42 PM

0 Likes
0
1852
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
‎2015-03-03 01:42 PM

Thanks Hal, probably too elaborate unfortunately, will require someone from their IT department to get involved, we try and avoid this when possible.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.