Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PM3255 Active energy into load

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • PM3255 Active energy into load
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
217
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
sesa250204
sesa250204 Leader
Leader

Posted: ‎2014-06-04 10:21 AM

0 Likes
4
2277
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
‎2014-06-04 10:21 AM

PM3255 Active energy into load

Hi all,

I have one problem using PM3255 on PME 7.2.1.

I don't have any informations about active energy into the load. I have standard log for Active out, Reactive in and out and Apparent in and out.

Also on Load report and tabular report I dont have data for Active energy. Still I have date for total active energy in and out before last reset.

Do I need to active it manually on meter? It is 300 km from my office, and I will be glad to solve it remotly.

Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 4
ganesh_azzo_com
ganesh_azzo_com
Troubleshooter

Posted: ‎2014-06-04 05:53 PM

0 Likes
3
2201
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
‎2014-06-04 05:53 PM

Hi Mario,

    

The first thing you can cross verify is , In PME 7.2 Active Energy into load is not default checked in MDI. Kindly try to tick the energy Into Load and see if you see data logging if not then you have to see in the meter  setup---->Log----> Energy Into load is “Enabled “.


Reply
JamesAZZO
JamesAZZO
Leader

Posted: ‎2014-06-06 08:03 AM

0 Likes
2
2201
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
‎2014-06-06 08:03 AM

You cannot enable the onboard flex log or configure it remotely. Normally this is where that measurement comes from.  Instead, just tick it in the MDI.

Reply
sesa250204
sesa250204 Leader
Leader

Posted: ‎2014-06-09 04:28 AM

0 Likes
1
2201
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
‎2014-06-09 04:28 AM

Thanks for the answer.

I did it through MDI, Active power into the load was not automatically checked.

One more question, how can we enable Load interval logging for day, week and the month?

Reply
Hal_Etheridge
Hal_Etheridge Champion
Champion

Posted: ‎2014-06-09 10:35 AM

0 Likes
0
2201
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
‎2014-06-09 10:35 AM

Just change the logging interval in the MDI for whatever period you want.  By default it should be logging every 15 minutes but this can easily be changed to whatever interval you wish.  The SW logging is controlled (in the driver) by a periodic timer with the same capability as the VIP (or the ION devices).
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.