Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Impulse meter m³ to m³/h - Power Monitoring Expert

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Impulse meter m³ to m³/h - Power Monitoring Expert
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
194
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
MathieuSA
MathieuSA
Explorer

Posted: ‎2025-06-06 12:06 AM

0 Likes
1
895
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
‎2025-06-06 12:06 AM

Impulse meter m³ to m³/h - Power Monitoring Expert

 

 Hello,

 

1) m³ Meters (GAS, WATER)
I have pulse meters that increment by 1 with each pulse.
• When creating dashboards, the visualization shows an already accumulated value.

MathieuSA_0-1749193031323.png

 

• Is it possible to display the consumption between two points in time (e.g., between N and N+1), in order to see the actual consumption over a given period?

 

2) Arithmetic Formulas
Is it possible to create calculations based on multiple measurements to obtain a new one?
I heard this could be done using Designer, but I’m unable to read my non-Schneider devices.

 

3) Manual Entry of Custom Data
Can we manually input a value (for example, a quantity in tonnes) directly within the PME interface?
• The goal would then be to use this data to display, in the dashboards, a consumption per tonne.

 

Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Romain_Polette
Romain_Polette Champion
Champion

Posted: ‎2025-06-10 07:53 AM . Last Modified: ‎2025-06-10 07:55 AM

0 Likes
0
871
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
‎2025-06-10 07:53 AM

Hello @MathieuSA , 

I read on the Power Meter forum, that your device is a Socomec (😢) and you created a custom Device Type.

 

1> m³ Meters (GAS, WATER)

Data on your dashboard seems not correctly aggregated.

When using the Device Type Editor -> did you select a Measurement known from PME ?

Romain_Polette_0-1749566241945.png

 

If you select a Water or Gas volume in the Measurement Tree of the DTE, your dashboard's data will be correctly aggregated (delta from N+1 to N = cumulative data like kW/h).

If you created a custom measurement, there is a chance that metadata associated to your Measurement are incorrect (you can update your metadata but this require SQL knowledge):

  • https://community.se.com/t5/EcoStruxure-Power-Monitoring/PME-2023-Custom-measurement-Not-showing-at-...
  • https://community.se.com/t5/EcoStruxure-Power-Monitoring/PME-Dashboard-data-issue/m-p/478895
  • https://community.se.com/t5/EcoStruxure-Power-Monitoring/Changing-Pie-Chart-Data-Aggregation-from-Su...

2) Arithmetic Formulas

This is possible to implement formulas inside the PME Virtual ION Processor (through Designer application).

Please read the ION Reference Guide for more info.

 

3) Manual Entry of Custom Data

This is possible to do it:

  1. Create a Ext Num object on VIP. This kind of object can be used to make calculation with ART Module for example.
  2. Use this object on PME Vista or PME Graphics Editor to enter your value.

Regards, 

 

Romain POLETTE
Solution Architect - France Operations

See Answer In Context

Reply
Reply 1
Romain_Polette
Romain_Polette Champion
Champion

Posted: ‎2025-06-10 07:53 AM . Last Modified: ‎2025-06-10 07:55 AM

0 Likes
0
872
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
‎2025-06-10 07:53 AM

Hello @MathieuSA , 

I read on the Power Meter forum, that your device is a Socomec (😢) and you created a custom Device Type.

 

1> m³ Meters (GAS, WATER)

Data on your dashboard seems not correctly aggregated.

When using the Device Type Editor -> did you select a Measurement known from PME ?

Romain_Polette_0-1749566241945.png

 

If you select a Water or Gas volume in the Measurement Tree of the DTE, your dashboard's data will be correctly aggregated (delta from N+1 to N = cumulative data like kW/h).

If you created a custom measurement, there is a chance that metadata associated to your Measurement are incorrect (you can update your metadata but this require SQL knowledge):

  • https://community.se.com/t5/EcoStruxure-Power-Monitoring/PME-2023-Custom-measurement-Not-showing-at-...
  • https://community.se.com/t5/EcoStruxure-Power-Monitoring/PME-Dashboard-data-issue/m-p/478895
  • https://community.se.com/t5/EcoStruxure-Power-Monitoring/Changing-Pie-Chart-Data-Aggregation-from-Su...

2) Arithmetic Formulas

This is possible to implement formulas inside the PME Virtual ION Processor (through Designer application).

Please read the ION Reference Guide for more info.

 

3) Manual Entry of Custom Data

This is possible to do it:

  1. Create a Ext Num object on VIP. This kind of object can be used to make calculation with ART Module for example.
  2. Use this object on PME Vista or PME Graphics Editor to enter your value.

Regards, 

 

Romain POLETTE
Solution Architect - France Operations
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.