Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION8650 default Alt PT and Alt CT ratios

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.

Search in

Improve your search experience:

  • Exact phrase β†’ Use quotes " " (e.g., "error 404")
  • Wildcard β†’ Use * for partial words (e.g., build*, *tion)
  • AND / OR β†’ Combine keywords (e.g., login AND error, login OR sign‑in)
  • Keep it short β†’ Use 2–3 relevant words , not full sentences
  • Filters β†’ Narrow results by section (Knowledge Base, Users, Products)
cancel
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
Showing results forΒ 
ShowΒ Β onlyΒ  | Search instead forΒ 
Did you mean:Β 
  • Home
  • Schneider Electric Community
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • ION8650 default Alt PT and Alt CT ratios
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
MatthewP
MatthewP Troubleshooter
Troubleshooter

Posted: β€Ž2014-06-13 02:12 PM

0 Likes
1
1385
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
β€Ž2014-06-13 02:12 PM

ION8650 default Alt PT and Alt CT ratios

While creating a custom framework on a ION8650A for the first time I noted the new scaled operational values feature.

The default alt PT and CT Pri/Sec values are 600/120 and 1/1 respectively. It would nice if this was set to a 1:1 ratio.

In my case I had to create a custom framework for a utility company where all meters  are sealed and are programmed with a PT or CT ratio of 1:1.

In the new frameworks, if the ratio is 1:1 the Alt ratios will take effect. We should not assume that 600:120 is awlays the case. Unless the meter tech knows about this feature, they may think something is wrong with the meter. Hence why I believe setting this to 1:1 out of the box is a good idea.

Also having the ability to change the alt scaling values from the front panel would nice. Quickly scrolling through the 8650 setup menus I didn't see anything jump out at me. If its there could someone please point where this is?

Lastly ION Setup 3.0 setup assistant does not have a menu screen to program these facroty module settings either. You have to dive right in to the Advanced configuration mode and configure the factory module.

Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Reply 1
sesa64419
sesa64419 Leader
Leader

Posted: β€Ž2014-07-03 09:32 AM

0 Likes
0
1347
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
β€Ž2014-07-03 09:32 AM

The scaled operational values feature was designed to only be configured/viewed/used through the Vista component of ION Enterprise/StruxureWare Power Monitoring Expert. It was created to allow operators to generate scaled values for their own power quality analysis from existing, non-configurable revenue-locked/sealed meters where the scaling ratio was set 1:1. This is why the scaled operational values feature configuration is specific to the Power Quality tab in Vista, and scaled operational value data is only intended to be accessed through ION Enterprise/StruxureWare Power Monitoring.

This feature was originally created on the ION8600 firmware v330, so you should see this on the later ION8600 as well as the ION8650.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.

Register today for FREE

Register Now

Already have an account? Login

Terms & Conditions Privacy Notice Change your Cookie Settings Β© 2026 Schneider Electric

Welcome!

Welcome to your new personalized space.

of

Explore