Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION 8800 DHCP

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • ION 8800 DHCP
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
sesa9650_bridge
sesa9650_bridge Explorer
Explorer

Posted: ‎2016-09-01 07:50 AM

0 Likes
3
1320
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
‎2016-09-01 07:50 AM

ION 8800 DHCP

ION 8800 with Ethernet comms can support DHCP from window server2012R2 without the need to change the IP addres manually at the site?

Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 3
Sanjeet_Sahota
Sanjeet_Sahota Mentor
Mentor

Posted: ‎2016-09-01 09:37 AM

0 Likes
2
1275
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
‎2016-09-01 09:37 AM

Hello Jaime,

The ION8800 does not support DHCP at this time.  Unfortunately, the meter will have to have the IP address changed manually.  If the meter can be accessed remotely (i.e. it is available on the network) via ION Setup, the IP address can be changed in the Comm Settings.  Please note though, that changing the IP address over ethernet will cause the user to lose communication VIA ION Setup and will need to reconnect using the NEW IP.  I would not recommend this, should the user accidentally set an IP that cannot be connected to, but it is definitely an option that is available.

Regards,

Sanjeet

Reply
sesa9650_bridge
sesa9650_bridge Explorer
Explorer

Posted: ‎2016-09-01 09:54 AM

0 Likes
1
1275
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
‎2016-09-01 09:54 AM

Hi Sanjeet,

Thank you for your clear answer. Do you know if there is a project in the near future to implement DHCP? or if there is a specific reason for not do it? This would help a lot to explain the customer,

Best regards,

Jaime

Reply
Sanjeet_Sahota
Sanjeet_Sahota Mentor
Mentor

Posted: ‎2016-09-01 10:29 AM

0 Likes
0
1275
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
‎2016-09-01 10:29 AM

Hi Jaime,


For the ION8800 as of right now I cannot say if there is a project in the future for it. There is no specific reason not to do it as far as I am aware, but cannot comment on whether it will be done in the future.  I will discuss with the OM if there has been other requests for this, but ultimately, they own the product roadmap and future evolution and will decide if/when they will add this feature.

Regards,


Sanjeet
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.