Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

FAQCommissioning How can I check if the Injection signal sent by IMD does go in a feeder monitored by a Locator?

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • FAQCommissioning How can I check if the Injection signal sent by IMD does go in a feeder monitored by a Locator?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
Madleen_Laclef
Madleen_Laclef Mentor
Mentor

Posted: ‎2015-03-05 10:57 AM . Last Modified: ‎2020-04-20 06:10 AM

0 Likes
0
960
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
‎2015-03-05 10:57 AM

FAQCommissioning How can I check if the Injection signal sent by IMD does go in a feeder monitored by a Locator?

One idea is to simulate an insulation fault on the feeder monitored by the XD312.

This would have to be a low insulation fault, around 1kOhm maxi.

The IM400 will go in alarm, most of its injection signal will go in the faulty feeder, and the XD will go in alarm, with the appropriate feeder LED active.

Like this you can validate that the injection of IM400 goes in the feeder; and you also validate the proper wiring of XD312 toroid.

 

 

To simulate this insulation fault, it means that you would connect a resistance of about 1kOhm between the network and the earth (downstream the feeder that you want to check). This resistance would have to stand the voltage of the installation (300V mini). It has to be placed in a ventilated environment, as it may heat.

When doing this test, ensure that the IM400 is not already in alarm... otherwise it would mean that you are creating a second insulation fault on the customer network... and protections will trip.

Labels
  • Labels:
  • Insulation Monitoring
Tags (2)
  • Tags:
  • commissioning
  • faq
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 0
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.