Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

FAQ _ Can Vigilohm be used to perform the Insulation Resistance Test as per the IEC 60364-6 standard?

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • FAQ _ Can Vigilohm be used to perform the Insulation Resistance Test as per the IEC 60364-6 standard?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
Madleen_Laclef
Madleen_Laclef Mentor
Mentor

Posted: ‎2015-07-29 05:56 AM . Last Modified: ‎2020-04-20 05:17 AM

0 Likes
0
967
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
‎2015-07-29 05:56 AM

FAQ _ Can Vigilohm be used to perform the Insulation Resistance Test as per the IEC 60364-6 standard?

This standard refers to an Insulation Resistance Test of the electrical installation.

7122

It is a common question whether the Vigilohm IMDs can be used to do this test.  The answer is NO, for this test what we use is a Megohmmeter.

 

Read this document to learn more about it.

Labels
  • Labels:
  • Insulation Monitoring
Tags (2)
  • Tags:
  • insulation
  • resistance
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 0
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.