Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Does ION7400 comply with EN62056 or IEC1107?

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • Does ION7400 comply with EN62056 or IEC1107?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
217
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
sesa101781_brid
sesa101781_brid Contributor
Contributor

Posted: ‎2017-05-31 05:20 AM

0 Likes
1
1091
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
‎2017-05-31 05:20 AM

Does ION7400 comply with EN62056 or IEC1107?

Hi Expert,

I got specification which requests the meter to have IR port which is complied with EN62056 or IEC1107. I can't find those standard in technical sheet but only found ANSI C12.18 & ANSI C12.19 instead. Please help to feedback if ION7400 (or others) those have IR port which is complied with EN62056 or IEC1107 standard.

Thank you very much

Chonnapan / PAE-Power Solution / Thailand

Tags (5)
  • Tags:
  • ansi c12.18
  • ansi c12.19
  • en62056
  • iec1107
  • iec61107
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Reply 1
Anonymous user
Not applicable

Posted: ‎2017-05-31 08:48 AM

0 Likes
0
1074
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
‎2017-05-31 08:48 AM

SANDRA PEDRO​ - can you comment?
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.