Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84244members
353343posts

Both Modbus and Ethernet ports

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

ahelizon
Crewman
Crewman
0 Likes
8
593

Both Modbus and Ethernet ports

Hi there,

I'm currently testing both PM8000 series and PM5500 series meters, daisy-chaining them on an Ethernet network. I have both meters connected to the server (laptop).

My question is - will both meters be able to handle two stacks of data at the same time? The requirement is that I use Modbus AND Ethernet at the same time, as they need to be hooked up to two different monitoring systems.

Also, PM5500 strangely changes its IP address when it's disconnected and connected back. Usually, it just updates to 255.255.255.255, something I can't understand.

Thanks in advance for your answers!

8 Replies 8
Bojan
Captain Captain
Captain
0 Likes
1
472

Re: Both Modbus and Ethernet ports

Hi Alex,

I connected one PM8000 as one Ethernet and one MODBUS over Ethernet Gateway meter at the same time in one PME 8 yesterday.

Best Regards,

daniel_parker_p
Lieutenant
Lieutenant
0 Likes
5
472

Re: Both Modbus and Ethernet ports

Hi Alex,

We've had that issue with the PM5500... it is strange!  It was fixed by power cycling it for us.  (I can find out the f/w vn if you like).

Not sure about your main question (only to say it "should" work). We have implemented an ION7650 talking via both Serial and Ethernet ports to separate systems at once.

ahelizon
Crewman
Crewman
0 Likes
0
472

Re: Both Modbus and Ethernet ports

That's perfect. The only question remaining is whether or not I could daisy chain it via Ethernet with PM5500 series?

Thanks Bojan,

Alex

Yu_Diao
Commander Commander
Commander
0 Likes
1
472

Re: Both Modbus and Ethernet ports

I ran into a similar situation for 10+ PM8ECC card installed on PM800 meters on one site. The IP reverted back to factory default and came back after a control power reset. We ended up to upgrade to a beta FW (back then), and they hold up well.

Not sure if they are related or not, I would suggest to upgrade to latest FW. If it persists, report to tech support.

Regards,

ahelizon
Crewman
Crewman
0 Likes
2
472

Re: Both Modbus and Ethernet ports

It is strange indeed. Please, do, it would be very helpful.

Also, I do realize that ION7650 can be easily implemented in that way, talking to both PMS and EAS (for example), however, it's the specs that hold me down - I need to know whether or not will both PM8000 and PM5560 support two stacks at once.

Thanks anyway so far Daniel,

Alex

ahelizon
Crewman
Crewman
0 Likes
0
472

Re: Both Modbus and Ethernet ports

That's perfect. It might be the issue, indeed.

Thanks Yu!

sesa56314
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
0
472

Re: Both Modbus and Ethernet ports

Hi Alex,

Both meters are able to handle two stacks of data at the same time.  You can have Ethernet (Modbus-TCP/IP, HTTP, FTP) at the same time as Modbus serial  (up to 32 devices ).


Thanks,

Art Wynans

daniel_parker_p
Lieutenant
Lieutenant
0 Likes
0
472

Re: Both Modbus and Ethernet ports

Hi Alex,

For the PM5560 we were on F/W version 2.0.1.

Daniel