Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Accusine PCS+ Settings to achieve both Harmonic Filtering and Power Factor Correction

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • Accusine PCS+ Settings to achieve both Harmonic Filtering and Power Factor Correction
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
Anonymous user
Not applicable

Posted: ‎2019-05-20 10:28 PM . Last Modified: ‎2020-12-02 03:31 AM

0 Likes
1
1542
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
‎2019-05-20 10:28 PM

Accusine PCS+ Settings to achieve both Harmonic Filtering and Power Factor Correction

Dear Team,

 

We have a case wherein we need to allocate for both Harmonic Filtering and PF Correction. We intend to set the priority as 100% to Active Harmonic Filtering and 0% to PFC Correction. As per the tabulation and explanation provided in the manual, we are understanding that 

 

"With Harmonic priority set to 100% the unit will output all current necessary to correct the harmonic content. Any output capacity left over will be used to correct PF and/or load balancing:

 

In our project the requirement is of 1004A as per the simulation study. We need to provide  300A: 3 Nos, 200A: 1 No. totalling to 1100A.

 

So based on 100% Filtering priority, once the requirement of 1004A is reached, will the unit deliver for Power Factor Correction the balance current available.

 

Alternatively whats the operation philiosohpy if we use the 90% Filtering and 44% Correction settings

Labels
  • Labels:
  • Power Quality
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Reply 1
Anonymous user
Not applicable

Posted: ‎2019-05-20 10:28 PM

0 Likes
0
1541
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
‎2019-05-20 10:28 PM

 
Attachments
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.