Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84426members
353616posts

trouble in applied signal in analog input of m221 logic controller

Machine Automation Forum

A forum addressing machine automation solutions for the complete machine lifecycle. Including offers like Machine Advisor, Modicon PLC/PacDrive, Lexium or Preventa. Discuss and share knowledge on offers relating to cloud-based service platforms, machine localization and monitoring, industrial operations control, motion products as well as safety function!

YanuarBob5150
Cadet
0 Likes
1
1093

trouble in applied signal in analog input of m221 logic controller

i have design simple i/o reading using so machine. i use so machine software to create ladder, making configuration and download pc to controller. After download i try to simulate by means of applied signal 0 to 10 Vdc to IN0 which have default setting (signal input range : 0 to 10 Vdc, scale : 0 to 1000). Actually when i applied signal to IN0, only signal 0 to 1.4 Vdc can be applied.

Can somebody help me to solve this?

1 Reply 1
sesa471789_brid
Ensign Ensign
Ensign
0 Likes
0
1025

Re: trouble in applied signal in analog input of m221 logic controller

Please share us the sample backup and the wiring done for the controller