Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84384members
353569posts

"Child Lock" Screen on TM172DCLxxx

Machine Automation Forum

A forum addressing machine automation solutions for the complete machine lifecycle. Including offers like Machine Advisor, Modicon PLC/PacDrive, Lexium or Preventa. Discuss and share knowledge on offers relating to cloud-based service platforms, machine localization and monitoring, industrial operations control, motion products as well as safety function!

Solved
sardila
Ensign
Ensign
0 Likes
2
614

"Child Lock" Screen on TM172DCLxxx

Hi Guys,

 

I am planning to implement a "Child lock" screen or lock screen after a x period of inactivity. I have an idea using the backLight timer to trigger a local timer which launch a pop-up screen which I design already. My question is in regards the system flag or timers documentation. I haven't found a proper documentation about those topics. Any ideas??? 

 

I much appreciate your suggestions,

 

 

Tags (1)

Accepted Solutions
Bastian_Schmitz
Commander Commander
Commander
0 Likes
1
611

Re: "Child Lock" Screen on TM172DCLxxx

You can find in the follow link an example how you could start a procedur regarding to inactivity

 

Example check for inactivity 

 

And you could check in you code the value of sysBacklight.

0 = Min Backlight active

1 = Backlight on

2 = Timer are running

 

You can adjust the time for sysBacklight via Par_BackLIghtTime

 

 

 

 

 

See Answer In Context

Tags (1)
sardila
Ensign
Ensign
0 Likes
0
571

Re: "Child Lock" Screen on TM172DCLxxx

Hi,

 

Thanks for your advise. Finally, I used a structure call  sysLCDPressed which triggers a timer. I could not find any documentation about this, I just tried and worked.

 

 
timer_LCD_Lock(IN:=NOT sysLCDPressed.is_LCD_pressed,PT:=60000);
 
if timer_LCD_Lock.Q then 
var_chck := Video_SendEvent (kWM_KEY, kKEY_VK_F8); 
end_if;
 
Thanks

See Answer In Context

Tags (1)
2 Replies 2
Bastian_Schmitz
Commander Commander
Commander
0 Likes
1
612

Re: "Child Lock" Screen on TM172DCLxxx

You can find in the follow link an example how you could start a procedur regarding to inactivity

 

Example check for inactivity 

 

And you could check in you code the value of sysBacklight.

0 = Min Backlight active

1 = Backlight on

2 = Timer are running

 

You can adjust the time for sysBacklight via Par_BackLIghtTime

 

 

 

 

 

Tags (1)
sardila
Ensign
Ensign
0 Likes
0
572

Re: "Child Lock" Screen on TM172DCLxxx

Hi,

 

Thanks for your advise. Finally, I used a structure call  sysLCDPressed which triggers a timer. I could not find any documentation about this, I just tried and worked.

 

 
timer_LCD_Lock(IN:=NOT sysLCDPressed.is_LCD_pressed,PT:=60000);
 
if timer_LCD_Lock.Q then 
var_chck := Video_SendEvent (kWM_KEY, kKEY_VK_F8); 
end_if;
 
Thanks
Tags (1)