Machine Automation Forum
A forum addressing machine automation solutions for the complete machine lifecycle. Including offers like Machine Advisor, Modicon PLC/PacDrive, Lexium or Preventa. Discuss and share knowledge on offers relating to cloud-based service platforms, machine localization and monitoring, industrial operations control, motion products as well as safety function!
Posted: โ2020-01-21 03:01 AM . Last Modified: โ2020-10-06 06:38 AM
Link copied. Please paste this link to share this article on your social media post.
Posted: โ2020-01-21 03:01 AM . Last Modified: โ2020-10-06 06:38 AM
Hello,
Does anyone have experience with configuring the XUPH001 in PLC mode?
This is the communication module for a pick-to-light system.
I'd like to connect it to a Modicon controller (e.g. M241) through a MODBUS connection.
How to configure the READ/WRITE holding registers, how to configure the system?
I'v read the manual, but do not fully understand... ๐
Can anyone provide me with some example code to get started?
Is there a function block available for this module?
Many thanks,
Best regards,
Mr. Tape
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: โ2020-02-02 07:30 PM
@Anonymous user Hi,
You can use IO Scanning instead of using Function Block in M241. it is more easier if you are new with Machine Expert (v1.1).
I will share it in video after this.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: โ2020-02-02 08:07 PM
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: โ2020-02-03 12:33 AM
Hello Sir,
I've done about the same in SoMachine... I only need to configure the IP and the unit ID....
Then I get the Device inputs and outputs...
The question still is how to read e.g. the status of the sensors, or activate the LED's in the sensors...
A programming example would be nice....
MAny thanks,
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: โ2020-02-03 01:35 AM . Last Modified: โ2020-02-03 01:42 AM
Hi @Anonymous user
I'm not familiar with XUPH001.
but after read the manual, if you already set to PLC mode. you can read from register that you mentioned (%MW18,19,20,21).
for direct access to bit, you can access/read from %IX and %QX for WRITE or you can map it to variable (recommended)
and here is the example to read status from sensor, then latch it 2 seconds to light on LED status
if you need to check the program: example code - machine expert 1.1
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.