Posted: 2022-07-19 03:44 PM
TM2 Module on M221 PLC
Can I use TM2 modules in M221 PLC without TM3 module. Thanks
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
Posted: 2022-07-21 10:59 AM
SE FAQ says no
https://www.se.com/ww/en/faqs/FA235150/
but you could configure it in ESME Basic and you could start it without an error in simulation.
I did not have a TM2 modul for test. I would suggest try it.
I could not find in the actual hardware hanbook the information that it is impossible.
- Tags:
- english
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
Posted: 2022-07-22 04:53 AM . Last Modified: 2022-07-22 09:06 PM
The Modicon M221 logic controller is for application for controlling of simple machines and offers best-in-class performance. It requires minimal installation and offers tremendous versatility. Connect a simple remote operator panel for instant maintenance and machine visualization.. facetime for windows
- Tags:
- english
Link copied. Please paste this link to share this article on your social media post.