Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84522members
353758posts

Error reading parameter 20048 - 20061 of M172 HVAC

Machine Automation Forum

A forum addressing machine automation solutions for the complete machine lifecycle. Including offers like Machine Advisor, Modicon PLC/PacDrive, Lexium or Preventa. Discuss and share knowledge on offers relating to cloud-based service platforms, machine localization and monitoring, industrial operations control, motion products as well as safety function!

HOANGTHINH
Lieutenant JG
Lieutenant JG
5
2231

Error reading parameter 20048 - 20061 of M172 HVAC

Hi all,

  I have a problem when I refresh page to read parameter of TM172, but it fail.

Who can help me ?

 

Picture1.png

 

Thanks for watching

5 Replies 5
Omaelk
Administrator Administrator
Administrator
2
2221

Re: Error reading parameter 20048 - 20061 of M172 HVAC

@MaPundir , you may be able to help @HOANGTHINH ? 😉

 

 

sesa471789_brid
Ensign Ensign
Ensign
1
2212

Re: Error reading parameter 20048 - 20061 of M172 HVAC

Hello ,

 

Please raise a bfo case with program backup and the firmware of the M172P , As this not a known issue and we have to check and analyis the same.

 

Best Regards

Bastian_Schmitz
Commander Commander
Commander
0 Likes
0
295

Re: Error reading parameter 20048 - 20061 of M172 HVAC

Hello the register address 20048 is in the range of the standard  EEPROM values.

The EEPROM values on TM172 could be in the range of 16384...20479.

Please check if you have values in this range and check which typ you have defined.

Maybe this could help to anayse the problem. 

Additional an information about the used ESME HVAC Version and BIOS Version could be helpfull.

 

Tags (1)
JacobJ
Crewman
Crewman
0 Likes
1
217

Re: Error reading parameter 20048 - 20061 of M172 HVAC

I am facing same issue I don't know what to do will you guys help me to solve

Subway Live IQ Login

Tags (1)
Bastian_Schmitz
Commander Commander
Commander
0 Likes
0
214

Re: Error reading parameter 20048 - 20061 of M172 HVAC

It is still necassary to knwo the target version which you select in your application, and to know which version is on the controller. Furthermore it would be important to know if you have EEPROM values in the range which generate the error.

 

WIthout this information it will be hard to solve the problem.

Tags (1)