Posted: 2023-05-19 01:13 AM
Connection 2 PLC and 2 HMI in different locations
Hi
I need advice on how to do a connection like that :
The PLC is TM251MESE, HMI's is XBTGT4330 and XBTGT7340
The buildings are about 200 meters apart, the biggest problem is how to add IP addresses from different network in HMI's.
I thinking about using IP Routing on TM521 but I don,t exactly how does work.
If there was a possibility add addresses from the same network in ETH1 and ETH2 thats solved the problem, but the addresses must be different.
Labels
- Labels:
-
Modicon M2xx
Link copied. Please paste this link to share this article on your social media post.
Replies 0