Posted: 2022-05-15 04:52 PM
Cannot connect to M241 over ethernet
Hello!
I unboxed new TM241CE24T/U and I upgraded Firmware to v5.1.9.21 for using with machine expert v2.0.
My problem is that I can connect to PLC over USB but not over Ethernet, even I can ping to its IP Address and I can access to Plc over web page.
Can You help me please ?
- Labels:
-
Modicon M2xx
- Tags:
- english
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
Posted: 2022-05-16 12:00 AM
Hi @MedSelmi ,
If you are trying to connect to the M241 via ethernet or USB it is important that the gateway is activated.
In the case of the Ethernet connection I always add the device ip address in the "Statis Remote Connections" like this:
The device it is shown as "Connected as client".
Verify also that your laptop/pc is in the same network as the controller.
Best regards,
Letomas
- Tags:
- english
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
Posted: 2022-05-16 12:00 AM
Hi @MedSelmi ,
If you are trying to connect to the M241 via ethernet or USB it is important that the gateway is activated.
In the case of the Ethernet connection I always add the device ip address in the "Statis Remote Connections" like this:
The device it is shown as "Connected as client".
Verify also that your laptop/pc is in the same network as the controller.
Best regards,
Letomas
- Tags:
- english
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
Posted: 2024-12-18 09:14 PM
why is mine always like this, i have been waiting for it for quite a long time but still can't connect
Link copied. Please paste this link to share this article on your social media post.