Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Webclient "There was an error trying to create the .NET control for this page"

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Webclient "There was an error trying to create the .NET control for this page"
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
3302 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Webclient "There was an error trying to create the .NET control for this page"

Picard Product_Support
‎2018-09-11 01:51 PM

Last Updated: Crewman ContentModerator ‎2025-09-25 03:23 AM

Issue

A dialog of "Cannot open .NET editor with .NET Framework" comes up with new installation of Webclient or after a Microsoft update of .NET 4.5.x.

There was an error trying to create the .NET control for this page.There was an error trying to create the .NET control for this page.There was an error trying to create the .NET control for this page.

Product Line

Andover Continuum

Environment

  • Continuum Webclient
  • Windows 7
  • Windows Server 2008
  • Windows 10
  • Internet Explorer

Cause

Microsoft changed the behavior of Internet Explorer when .net 4.5.x is installed on a PC. It turns off .net 2.0 support which is needed for several editors to function on Webclient browser PCs

Resolution

See web.Client v2.0 .Net Editor Hotfix on the EcoXpert Extranet This is a registry key file that installs the registry keys mentioned further down in this article. It allows Internet Explorer to utilize .net 2.0 that several webclient editors use.


This hotfix contains a .reg file which changes the registry, it is recommended to make a Windows Restore point or a backup (export) of the existing registry folder (hive).

The hotfix only updates the following keys, so the changes can also easily be made manually.

  1. On an 32-bit (x86) Operating System
    1. Add a DWORD attribute with the name EnableIEHosting to KEY_LOCAL_MACHINE\SOFTWARE\Microsoft\.NETFramework
    2. Set the value to 1
  2. On an 64-bit Operating System
    1. Add a DWORD attribute with the name EnableIEHosting to KEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Microsoft\.NETFramework
    2. Set the value to 1

A reboot of the webclient browser PC is required after the change is made. Each browser PC will need to have this fix applied.


Microsoft Edge can also be used on newer client PCs, see the following article:

Microsoft Edge can be used for webclient client PCs 

 

Labels (1)
Labels:
  • Andover Continuum
Tags (4)
  • Find more articles tagged with:
  • 17498
  • 4.5.1
  • AlanWood24
  • disabled
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.