Join our 30-minute expert session on July 10, 2025 (9:00 AM & 5:00 PM CET), to explore Digital Twins, cooling simulations, and IT infrastructure modeling. Learn how to boost resiliency and plan power capacity effectively. Register now to secure your spot!

SQL 2008 and Windows 7

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • SQL 2008 and Windows 7
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • Roger_Bently
    Roger_Bently
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1393 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

SQL 2008 and Windows 7

Picard Product_Support
‎2018-09-06 12:45 PM

Issue

Running SQL 2008 on a Windows 7 OS

Product Line

TAC INET

Environment

  • I/NET version 2.41
  • SQL 2008
  • Windows 7

Cause

SQL 2008 and I/NET version 2.41 on a Windows 7 PC.

Resolution

Note: Do not install Microsoft SQL Server 2008 Express Edition on the filemaster of an equalized TAC I/NET Seven system. This database engine does not provide the replication services that are required on the filemaster.

Microsoft SQL Server 2008 Express Edition is a scaled down, free edition of Microsoft SQL Server 2008, which includes the core database engine. While there are no limitations on the number of databases or users supported, it is limited to using one processor, 1 GB memory and 10 GB database files. Microsoft SQL Server 2008 Express is included on the TAC I/NET Seven installation disk in the SQLExpress folder (installation instructions are in the SQL2008 Expr Install Inst.pdf file included in the folder).

Microsoft SQL Server 2008 Express Edition does not provide the replication services that are required on the filemaster. To use Microsoft SQL 2008 as the SQL engine for an equalized TAC I/NET Seven system, install Microsoft SQL Server 2008 Standard Edition on the filemaster. You can then use Microsoft SQL Server 2008 Express Edition on each equalized client.

I/NET Seven supports the use of Microsoft SQL Server 2008 Express 32-bit Edition running on Windows 7 Professional 32-bit. The PC should have at least 2 gigabytes of RAM.

Microsoft SQL Server 2008 32-bit (see notes 1, 2, 3, and 5
  Freely Distributed with I/NET Maximum Database Size Maximum Concurrent Users Operating Systems Supported
SQL Server 2008 Express (32-bit) (See note 4) Yes 10 GB Unlimited Windows 7 Professional 32-bit
SQL Server 2008 Standard (32-bit) No Unlimited Unlimited Windows 7 Professional 32-bit
  1. Do not mix versions of SQL server among equalized or client/server workstations in your TAC I/NET Seven system. Ensure that the edition of SQL server installed on each workstation used in a client/server or equalized setting are based on the same version of Microsoft SQL, either 2000, 2005, or 2008
  2. It is strongly recommended that you defragment the PC’s hard drives on a regular basis. Severely fragmented hard drives can cause poor system performance and in some cases can introduce data errors.
  3. The use of Microsoft SQL Server 2005 Standard or Enterprise edition, or any edition of Microsoft SQL Server 2008 will require that the PC have at least 2 GB of RAM.
  4. Microsoft SQL Server 2005/2008 Express Edition cannot be used on a TAC I/NET Seven filemaster.
  5. Only 32-bit versions of SQL Server and Windows 7 Professional are supported.
Labels (1)
Labels:
  • TAC INET
Tags (1)
  • Find more articles tagged with:
  • 7191
Was this article helpful? Yes No
No ratings

Link copied. Please paste this link to share this article on your social media post.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.