Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Using STR-350 Bypass button as On/Off button in Classic Network

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Using STR-350 Bypass button as On/Off button in Classic Network
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • CraigEl
    CraigEl
  • sesa145087_brid
    sesa145087_brid
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2327 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Using STR-350 Bypass button as On/Off button in Classic Network

Picard Product_Support
‎2018-09-11 04:22 AM

Last Updated: Administrator CraigEl Administrator ‎2022-08-09 01:20 AM

Issue

Using STR-350 Bypass button as On/Off button in Classic Network

Product Line

TAC Vista

Environment

  • Vista
  • STR-350
  • STR-351

Cause

Sometimes on/off function is needed when using STR 350/351 to start or stop a device.

Resolution

Following the steps below to realize this function in Classic Network:

  1. Create a Menta file and Click "Add STR Module" in the Device Specification.
  2. In the Bits field of HVAC settings, change the value of the last 3rd bits of the first line from "0" to "1". This bit is to switch the using Bypass button as on/off function on.
  3. Create an STRIN and STROUT module. Bind the STRIN to OccManCmd variable, while bind the STROUT to EffectOccup.
  4. Connect the STRIN to an real DO point to control the start/stop of device. But an calculation is needed because when the button is off, the value is 2 while the button is on, the value is 3 instead of simple 0/1.
  5. Also connect the STRIN to STROUT to make the output synchronize with the input, like the program below. You can also download the sample from here.

For the application used in the LNS network, refer to the Using STR-350 Bypass button as On/Off button in LNS Network.

Labels (1)
Labels:
  • TAC Vista
Attachments
STR.ZIP
Tags (1)
  • Find more articles tagged with:
  • 12825
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.