Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Failed to create or configure database on SQL Server! ([17] SQL Server does not exist or access denied.)

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Failed to create or configure database on SQL Server! ([17] SQL Server does not exist or access denied.)
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
4591 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Failed to create or configure database on SQL Server! ([17] SQL Server does not exist or access denied.)

Picard Product_Support
‎2018-09-07 06:24 AM

Last Updated: Crewman ContentModerator ‎2025-08-11 03:59 AM

Issue

During a Vista 5.x.x installation, failure can occur during the SQL installation portion of the install.

This solution could encompass many different SQL installation errors; however, one that is known and verified is shown below:

Failed_to_create_or_configure.png


Failed to create or configure database on SQL Server! ([17] SQL Server does not exist or access denied.)

Here is another common one:

Failed to create or configure database.png

 

Failed to create or configure database in SQL Server ([1802] CREATE DATABASE failed. Some file names listed could not be created. Check related errors.)

If you have previously uninstalled Microsoft SQL Server, data files for the database may still exist in the SQL Server data directory.

Remove the files manually and click Retry or click Cancel to abort installation.

Product Line

TAC Vista

Environment

TAC Vista Server 5.x.x

Cause

  1. Uninstalling and reinstalling the software can leave pieces of SQL behind. Even if you try to uninstall everything in Add/Remove Programs, left over portions may cause the TAC Vista installation not to be successfully installed.
  2. The Program Files\SQL Server directory is flagged for compression or encryption.
  3. Installing Vista version below 5.1.5 on a Windows 7 64bit machine will cause this error.

Resolution

Please check the Windows Event log for the specific installation error. See Viewing, Saving, Sharing Windows Event Logs for Troubleshooting Purposes for information on viewing the Windows Event Log. Consult Log file of SQL installation when installing Vista Server for information on viewing the SQL Server installation log.

If the Event log reveals Error 28001, the sa password must meet SQL Server password policy requirements, please refer to the solution provided in Error 28001 - sa password complexity error when installing TAC Vista 5. If not, then please proceed with the resolution below:

If the SQL Server installation log file complains that the Program Files\SQL Server\ directory is flagged for encryption or compression then right click on the directory and select properties. The advanced option exposes the check boxes for compression and encryption. If the folder is flagged for compression the it will be visible in blue instead of black font. Remove the encryption or compression flags and apply then reinstall.

If the PC operating system is Windows 7 64-bit, install Vista 5.1.5 or higher. Resolution below will not solve the issue.

In most cases this is caused by MSXML 6.0 parser. This software is commonly installed by programs using SQL, and also during the TAC Vista installation. If this can't be removed using Add/Remove Programs, you can download a program from Microsoft that cleans up and removes this software (and others).

It is called Windows Installer Cleanup. Link to download: msicuu2.exe.
NOTE: Microsoft recently removed this utility from the downloads section of their support site. They have this to say about the utility:

While the Windows Installer Cleanup utility resolved some installation problems, it sometimes damaged other components installed on the computer. Because of this, the tool has been removed from the Microsoft Download Center.

Use this utility with care at your own risk.

Windows_Installer_Cleanup.png

 

In most cases TAC Vista will install successfully after removing MSXML 6.0 parser.

For alternative solutions see SQL Express install fails on MSXML 6 and Error when installing SQL 2005 Express on a machine that had previously had MSDE installed .

Labels (1)
Labels:
  • TAC Vista
Attachments
msicuu2.zip
Tags (1)
  • Find more articles tagged with:
  • 3926
Was this article helpful? Yes No
100% helpful (2/2)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.