Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84402members
353595posts

ST6500 webserver

Industry Automation and Control Forum

This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.

Solved
Sbracke
Crewman
Crewman
0 Likes
3
1304

ST6500 webserver

I enabled the webserver on my ST6500 HMI. When I tried to connect to the panel there was no web-page available (http error 404).

 

Is there a manual/example available for the webserver? The help-file in EOTE is , as always, very scarce with information.

Tags (1)

Accepted Solutions
Paul_Derbyshire
Ensign Ensign
Ensign
0 Likes
2
1290

Re: ST6500 webserver

Hello,

 

The ST6500 today only supports the Web API functionality.  This means writing your own code to use HTTP requests or websockets to access read only variables/alarms.  Still a web server but not for generic web page access.

 

When we offer version 3.2, which is expected in early 2021, you will be able to connect using a regular web browser and view the HMI screens using the Web GUI (Graphic User Interface) in synchronous mode.  Full read/write access should be available. 

 

Keep an eye out for version 3.2 :).

Paul Derbyshire
Senior Product Application Expert | Sales Enablement | HMI Line of Business, Digital Factory | Industrial Automation Business | Schneider Electric

See Answer In Context

Tags (1)
3 Replies 3
Paul_Derbyshire
Ensign Ensign
Ensign
0 Likes
2
1291

Re: ST6500 webserver

Hello,

 

The ST6500 today only supports the Web API functionality.  This means writing your own code to use HTTP requests or websockets to access read only variables/alarms.  Still a web server but not for generic web page access.

 

When we offer version 3.2, which is expected in early 2021, you will be able to connect using a regular web browser and view the HMI screens using the Web GUI (Graphic User Interface) in synchronous mode.  Full read/write access should be available. 

 

Keep an eye out for version 3.2 :).

Paul Derbyshire
Senior Product Application Expert | Sales Enablement | HMI Line of Business, Digital Factory | Industrial Automation Business | Schneider Electric

Tags (1)
YUSUFK
Lieutenant JG
Lieutenant JG
0 Likes
1
990

Re: ST6500 webserver

Dear Paul,

We would like to use Web GUI feature in the ST6400.

However, Do we have to use or order an API code to activate Web GUI?

If so, could you inform us about code and licence informations for WEBGUI?

Is it possible to use it as free or trial at the moment?

 

Thanks in advance.

Tags (1)
Sbracke
Crewman
Crewman
0 Likes
0
977

Re: ST6500 webserver

Hey,

 

I asked the same question to a schneider rep. recently and got this in response:

 

HMIWRT001    1    EOTE webviewer keycode - 1 pc      50,00 euros brut
HMIWRT010    1    EOTE webviewer keycode - 10 pcs   200,00 euros brut
HMIWRT100    1    EOTE webviewer keycode - 100 pcs    600,00 brut

discount code: TAK

 

Don't know if the prices are the same in your region but maybe this helps.

Tags (1)