Posted: 2023-03-30 03:14 AM
Mail sending from CitectSCADA
Tried to send email from CitectSCADA via MailLogon, MailSend and MailLogoff functions, but it isn't working. Are there any special requirements for this? Do I need to specially configure Microsoft Outlook? Could you please make an advice?
- Labels:
-
Connected Products
- Tags:
- english
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
Posted: 2024-05-24 11:30 AM
I had same issue. Got error code 276. Looks like no privilege to open outlook from Correct. Anything setting need to change in outlook?
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
Posted: 2024-05-24 01:21 PM
Just found need setup citect to allow exec to true to allow open outlook
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
Posted: 2024-07-02 01:32 AM
Hello
Two things.
1- Everyone of this functions have a return value. With this you can do a troubleshooting.
2- Remember that Citect/Plant SCADA is working with 32bits process, and then .... It is advisable to always work with 32-bit programs. If you have the option of installing it in 32-bit, it's the better.
For example, Thunderbird has a 32-bit version, if you don't install that version, sending emails doesn't work.
BR
Ricard
Link copied. Please paste this link to share this article on your social media post.