Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-04-26 04:01 AM
Hi all,
I currently read the PLC serial number via the variable name. I'd like to do this by reading the Modbus address. How can I do this?
If you look at the attached images you'll see the code using the full variable name which works, but I can't seem to get the Modbus read on the line below it to be accepted no matter what I do, yet I've seen it online (sods law I can't find it again even if I search my history).
Can somebody tell me the correct syntax structure for reading the system variables?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-04-28 01:05 PM
I'm assuming you are talking about an M241 PLC? Based on another entry in the help, it might not be %SW, but %MW. %MW60050 is i_byIPAddress, a read-only System Variable. Try %MW60002.
That said, there is a note in the help which says 60000 to 60034 are "not accessible through the application":
Compare against this, which specifies %MW, and is also a system read-only variable:
Have a play based on that and see what you get. Also try reading both of those registers directly via Modbus tester and see if they are available externally (assuming 60002 = %MW60002 = 460002 or 460003).
It is also possible it is neither %MW or %SW, and may just be the straight Modbus address where 6x is the 'Extended Registers' range that some devices support (but I have never used or seen used).
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-04-28 11:10 PM
Hi @MatthewM,
Many thanks for replying, much appreciated.
The PLC is an M251.
I can definitely read 60002 if I read by 'Var Name', so where it says ''Not accessible through the application'' I wonder if this means only the Modbus reads via %SW and/or %MW are not allowed for that variable.
I will try addressing the Modbus registers directly though as you suggest and report back.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-07-01 10:32 PM
To read system variables using their Modbus address instead of their names, you need to use the correct syntax in your PLC programming. Instead of referring to the variable by its name, you should use the Modbus address directly. Make sure the Modbus read command is formatted correctly for your PLC system. Sometimes, the syntax can be tricky, so double-check your code for any errors in how you're specifying the Modbus address. If you've seen examples online before but can't find them now, try checking your browsing history for reference. This approach should help you read system variables via Modbus effectively.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.