This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2022-12-0906:49 AM
This will depend on the controller that you are using and the communication method that you are using with Citect. The Analog Device DDT's in the Modicon M580 have a FORCED Status. If you are using the Schneider Electric OPC DA or UA server, you can gain access to this information directly.
This is a screen capture from the Analog Input Module.
This is a screen capture form the Analog Output Module.
For the Digital Input and Output you will need to use the IS_BIT_FORCED EF to detect the force status.
In addition, System Words %SW108 and %SW109 will provide a count of the number of forced digital and analog channels in the application.