Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84666members
354057posts

FREE TRIAL AVAILABLE - EcoStruxure™ Control Expert - Asset Link v2.1: Design tool for seamless integration of control and supervisory systems

Industry Automation and Control Forum

This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.

Rodrigo_Garcia
Administrator Administrator
Administrator

FREE TRIAL AVAILABLE - EcoStruxure™ Control Expert - Asset Link v2.1: Design tool for seamless integration of control and supervisory systems

 

EcoStruxure Control Expert – Asset Link v2.1 is now available on Exchange.

 

Schneider Electric strives to continuously improve customer satisfaction and user experience.

EcoStruxure Control Expert – Asset Link is a Software Integration tool to engineer Integrated Automation Systems based on Modicon controllers and AVEVA System Platform.

 

DOWNLOAD YOUR FREE TRIAL

 

Discover the functionalities

 

In-line Pattern Management

  •              User has the capability to Manage Pattern within the User Interface of AVEVA System Platform
  •              Smart definition (edit and refine) of Patterns can now be achieved using in-line editor without any need of XML Coding knowledge.

 

Support templates created using Object Wizard

  •              This release of Asset Link supports AVEVA System Platform templates created using AOT (Automation Object Toolkit) or Object wizard

 

Flexibility to Select Root Area and Area Templates

  •              Area templates enables user to pre-define conditions to add intelligence to assets under the area instances.
  •              This release of asset link enable user to select the Area templates during configuration when used with EcoStruxure Process Expert for AVEVA System Platform

Enhanced User Interface and Integrated Help

  •              This release brings improvised user interface and additional capabilities to refer to the integrated help for easy configuration and utilization of the Software.

 

Rodrigo G. 


Industrial Automation Community manager

1 Reply 1
Omaelk
Administrator Administrator
Administrator
0 Likes
0
449

Re: FREE TRIAL AVAILABLE - EcoStruxure™ Control Expert - Asset Link v2.1: Design tool for seamless integration of control and supervisory systems

thanks for sharing

Tags (1)