Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84382members
353566posts

Ecostruxure Operator Terminal Expert 3.2 How to access one bit of a Symbol linked memory word (i.e %MW10) to use for a switch variable?

Industry Automation and Control Forum

This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.

Solved
Steve_P
Crewman
Crewman
0 Likes
4
1541

Ecostruxure Operator Terminal Expert 3.2 How to access one bit of a Symbol linked memory word (i.e %MW10) to use for a switch variable?

Hi all, 

 

I know there is probably a simple solution, but I have searched everywhere for it and can't find the answer.

I have an existing M221 PLC running a STP,  which has a failing HMI that is in need of replacement (operator accident, damaged the screen) We have decided to replace it with a HMIST6500 screen and I'm in the process of changing over the code from the old Vijeo designer to the new EOTE code.

 

I have successfully set up the symbol link and have a list of all the tags with names etc - all good. However I have discovered that the M221 code has been written with a large proportion of the bool variables (eg, start, stop, manual, auto, forward, reverse etc) stored in words, with the idea that each word relates to a particular motor or pump.

 

However I have not been able to find out how to access these individual bits within the EOTE software, so far I have tried:

STPM221.Memory_Words.MW_10..3.Value

STPM221.Memory_Words.MW_10:3.Value

%MW10:X3

%MW10.3

 

All which do not work. I'm thinking that I will need to use a converter to isolate the required bit? Can someone please point me into the correct direction.

 

Also there were some rumours on one of the forums I was reading where it said that there is a Vigeo -> EOTE convertor in the pipeline - any news on this?

 

 

 

Tags (1)

Accepted Solutions
Bastian_Schmitz
Commander Commander
Commander
0 Likes
1
1513

Re: Ecostruxure Operator Terminal Expert 3.2 How to access one bit of a Symbol linked memory word (i.e %MW10) to use for a switch variable?

Hello,

The acces to a bit of a word is possible via Modbus FC Holding Registers through the Syntax

word.X0 = Bit0 of Word

...

word.X15 = Bit15 of Word

 

best regards

See Answer In Context

Tags (1)
4 Replies 4
Bastian_Schmitz
Commander Commander
Commander
0 Likes
1
1514

Re: Ecostruxure Operator Terminal Expert 3.2 How to access one bit of a Symbol linked memory word (i.e %MW10) to use for a switch variable?

Hello,

The acces to a bit of a word is possible via Modbus FC Holding Registers through the Syntax

word.X0 = Bit0 of Word

...

word.X15 = Bit15 of Word

 

best regards

Tags (1)
ismailozinan
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
1
1507

HelloRe: Ecostruxure Operator Terminal Expert 3.2 How to access one bit of a Symbol linked memory word (i.e %MW10) to use for a switch variable?

Hello,

You can find sample programme and video for %MW10:X1 at link.

this is Bit Toggle control via EOTE.

Best Regards,

Tags (1)
Steve_P
Crewman
Crewman
0 Likes
0
1500

Re: Ecostruxure Operator Terminal Expert 3.2 How to access one bit of a Symbol linked memory word (i.e %MW10) to use for a switch variable?

Thanks for your reply,

 

Yes, this will work, I knew there would be a simple approach. Just needed the right minds in the same room, Haha

 

Cheers

Tags (1)
Steve_P
Crewman
Crewman
0
1496

Re: HelloRe: Ecostruxure Operator Terminal Expert 3.2 How to access one bit of a Symbol linked memory word (i.e %MW10) to use for a switch variable?

Hi Ismailozinan,

 

Thanks for the reply, especially the effort you have put into the video. 

 

Appreciate your help

 

Both answers work well, just a matter of figuring out which suits my application best.

 

Great to get fast response from the Schneider Team. Cheers.

Tags (1)