Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-10-14 11:53 PM
Hi,
I am running Control Expert V15 SP1. If I start the simulator I can connect to it from Control Expert and download the program to it and monitor it and Control Expert stays connected. As soon as I try to connect to the simulator from another software package eg. Vijeo Designer, then Control Expert loses its connection to the simulator. Vijeo Designer is now connected with no problems and I can simulate the running PLC, but Control Expert will not connect again while the Vijeo Designer connection is active. I have to stop Vijeo Designer first before Control Expert will connect again to the simulator. It seems as if the simulator only allows one connection at a time.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-10-15 07:24 AM
Hi,
This was a known issues when you use the first release version of Control Expert V15.0 SP1. The PLC Simulator accept only one TCP connection.
Attached herewith is the Hotfix for the Control Expert V15.0 SP1.
Try this out and it should solve your issues.
With Regards,
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-10-15 07:24 AM
Hi,
This was a known issues when you use the first release version of Control Expert V15.0 SP1. The PLC Simulator accept only one TCP connection.
Attached herewith is the Hotfix for the Control Expert V15.0 SP1.
Try this out and it should solve your issues.
With Regards,
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-10-17 11:18 PM
Hi Michael,
The hotfix fixed the problem.
Thanks for the help.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-05-22 12:31 PM
Hi,
I'm running Control Expert V15.3 and trying to connect to the simulator with multiple connection, without success. Does version 15.3 have any hotfixes for this?
Regards,
Maura Carvalho
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-05-23 10:33 PM
Hi,
The PLC Simulator is limited to a single "Programming" connection mode, which is exclusive to programming and modification by the currently connected EcoStruxure Control Expert software. The remaining connections will be in the "Monitoring" connection mode.
Note that by specifying a different port number allows EcoStruxure Control Expert V15.0 and later to support several instances of the PLC simulator running on the same local host PC. For example, 127.0.0.1:503.
With Regards,
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-05-24 11:18 AM
Hi Michael.
I was now able to connect with local IP 127.0.0.1, but I would need to connect with an IP that could be read by another server. I understood then that with an IP different from the 127 it doesn't work.
I think I have to install ControlExpert on the same server as my supervision software.
Thank you.
Maura Carvalho
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-05-28 08:29 PM
Hi Maura,
With EcoStruxure Control Expert V15.0 and later, a new option has been introduced on PLC Simulator: the listening IP address (default = 127.0.0.1). The reason is used to avoid the PLC simulator reaching an external IP port due to cybersecurity.
For external communication, you will need to set this listening IP to 0.0.0.0 or assigned the IP address of its PC External port.
Why PLC Simulator can’t receive external communication ?
With Regards,
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-04-23 01:54 PM
Hello,
I tried to follow your procedure and set the listening IP address to 0.0.0.0, but I get an error message. (See photo.)
Can you help me, please?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-04-24 09:10 PM
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-04-27 10:28 PM
Hello,
I'm trying to get two VMs to communicate with each other.
One VM has Control Expert v15.2 installed, and the other has Vijeo Designer v6.2.12.24 installed.
My problem is that I can't simulate my PLC program with the HMI.
I searched the internet and came across a post on the Schneider forum titled: "Control Expert Simulator only allows one connection."
So I tried everyone's strategies, including yours, to resolve my problem without success. I still get the error message "Invalid PLC address or busy or media off."
Thank you in advance for your feedback.
Sincerely,
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.