Posted: 2020-03-24 10:26 PM
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
Posted: 2020-03-24 10:26 PM
Citect V7.40 SP1 Installation on Win 10
Hi,
I am wondering if anyone has tried installing Vijeo Citect V7.40 SP1 on Win 10?
On SE website, it is not clearly mentioned if Win 10 is supported.
I could install V7.40 and SP1 on Win 10 without any issues but when trying to open Citect Explorer, I am getting an error. Please refer to the attached screenshot.
Thank you!
- Labels:
-
Smart Design & Engineering
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
Posted: 2020-03-25 02:16 AM
Hi
Looking on the AVEVA support site, it looks as though this version Citect Scada is not supported on Win 10.
OS Environment Compatibility for V7.40 SP1 is
Windows 7 SP1 Professional (x64, x86)
Windows 8 Enterprise (x64, x86)
Windows Server 2008 SP2 Enterprise (x64, x86)
Windows Server 2008 R2 SP1 Enterprise
Windows Server 2012 Standard
Is there a reason why you need this specific version Of Citect Scada ?
There are usually many benefits to upgrading to a later version.
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
Posted: 2020-03-25 03:40 AM
Its worth double checking the Citect.ini file,
In the section [CtEdit] ensure all the paths are correct, pay particular attention to
- Bin: folder which should point to the Citect installation folder location, it has Citect32.exe
- User: which has all the Citect projects, see the attached screenshot
The following is a example INI setting for Citect SCADA 2018,
[CtEdit]
Bin = C:\Program Files (x86)\Schneider Electric\Citect SCADA 2018\Bin
Config =C:\ProgramData\Schneider Electric\Citect SCADA 2018\Config
Data =C:\ProgramData\Schneider Electric\Citect SCADA 2018\Data
Logs =C:\ProgramData\Schneider Electric\Citect SCADA 2018\Logs
User =C:\ProgramData\Schneider Electric\Citect SCADA 2018\User
Regards
Rob
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
Posted: 2020-03-25 04:05 AM
Also check the Master.dbf, which is found in the User location, it contains the project name and project location, ensure that the folder locations for each project are correct.
I have attached an example screenshot. NOTE do not change the column widths
Regards
Rob
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
Posted: 2020-03-25 05:52 PM
Hi Stevey,
Thanks for your reply. One of my clients is using citect v7.40 SP1 on Win 7 and now Microsoft has stopped supporting this version of OS. Thus I was wondering if we could install the same version of Citect on Win 10 instead of upgrading their Citect to the latest version.
Cheers!
Singh
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
Posted: 2020-03-26 02:23 AM . Last Modified: 2022-05-18 07:53 AM
Hi Singh
OK, I understand. It's not officially supported and so there's no guarantees that this combination would perform correctly.
Upgrading to the latest version should be pretty easy as there has been a lot of work put in to improving the upgrade process. Obviously if the system isn't in a support contract then there would be a cost for the license upgrade.
For more information, you can reference the Citect 2018 – Upgrading to Citect SCADA 2018 PDF, which shows that you can go directly from 7.40 SP1 to 2018. Should be applicable for 2018 R2 as well.
Hope this helps
Stevey
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
Posted: 2020-03-31 03:58 AM
No worries, Thanks Rob.
Cheers!
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
Posted: 2024-07-03 02:24 AM
Hello,
Sharing my experiences in this topic.
I had a project where we had to move the Citect 7.40 Application to a new Windows 10 Server. Because the Software License is so expensive for the upgrade, the customer requested using 7.40.
However, I managed to set up Citect 7.40 on Windows 10. It has been running with no problems for a year.
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
Posted: 2024-11-27 03:55 PM
Hi Thomas,
Could you please share how you made it? Thanks.
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
Posted: 2025-02-21 10:29 PM
hello everyone, I have problem with installing Vijeo Citect 7.4, I cannot find link where I can download, can everyone help me how to download Vijeo Citect 7.4
Link copied. Please paste this link to share this article on your social media post.