Industry Automation and Control Forum
This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-07-11 06:56 AM
Dear All,
I have never work with Citect SCADA, and las days i had to convert a PC (where the Citect V6.0 is installed) in Virtual machine.
The SCADA is connected with a SIEMENS PLC S7 315-2DP via Ethernet.
The vistual machine works fine, but the SCADA cannot connect to PLC. I gues there is something in connection settings, But i don´t know where is it.
All computer name and IP address are the same, only the network card name has been changed.
Please help me how to setup the connection between the Citect and PLC.
Thank you and best regards.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-07-11 09:25 PM
Hi, Which driver is the Citect setup to use? PSDirect or S7NT? (To check open Citect Explorer, Change to the Project Editor Menu Communications>IODevices
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-07-12 05:33 AM
Hi, Thank you for the comment.
It uses S7NT driver.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-07-14 10:10 PM
The S7NT driver uses the Simatic Net software from Siemens to connect to the PLC. Did you check the Simatic Net is still licensed on the virtual machine and configured?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-07-17 04:35 AM
I have check the Simatic PG/PC interface and it is OK.
I can connect the PLC with SIMATIC MANAGER.
Please check the photos of the settings.
Thank you.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-07-17 10:10 PM
Hi, All the info above seems correct but need the NetPRO configuration as well to be sure.
Once the configuration is complete in NetPro, it must be transferred to the PC Station. This can either be done by a file or over the Network. Provided that everything is OK, you should see your configuration from NetPro appear in the Station Configuration Editor on the Local PC.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-12-18 06:57 AM
Dear Hennie,
Thank you for your reply.
Regarding the NetPRO configuration, I am not sure if everything is OK there.
In the Simatic manager, it is configured. Please find a photo of that.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-01-09 11:43 PM
Hi, You need to add a PC Station in NetPro and set as type Application. Netpro must be installed and running on the Citect IO Server. After you configured the PC Station in Netpro you need to download it as well (same process as downloading to PLC. See attaced screenshot of the fields in NetPro and where they must correspond in the Citect configuration.
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.