Posted: 2024-05-30 04:06 PM
BMENOC0301 | What is the default Ethernet communication port?
Hello, I'm trying to communicate a M580 with a BMENOC0301 module with a third party device. I'm trying to use the "DATA_EXCH" function configured to send a unconnected message through CIP protocol. The third party device has an option to change the port for TCP communication. Do you know what is the default port for the Schneider device for this type of communication? (For example I know that modbus default port is 502). Is there a way to change it? Thanks in advance.
Labels
Link copied. Please paste this link to share this article on your social media post.
Replies 0